Roof Mounted Fans-FAQQA5
What factors prevent fans from not performing as specified?
Unique title :
Roof Mounted Fans-FAQQA5
Select a Card/Question Answer :
QuestionAnswer
Display order :
5
There are numerous reasons why fans fail to perform as specified. But first it is important to understand what defines acceptable performance. According to AMCA Publication 200, a fan installed in a ventilation system should expect a tolerance of +/- 7.5% for flow (cfm). In other words, a fan that produces 1,000 cfm in a lab environment should provide a volume flow rate of 925 to 1,075 cfm when installed in a properly designed ventilation system. Volume flow rates falling below this range are typically the result of variances in system static pressure or mechanical problems with the fan.
Common symptoms include:
- Obstructions in the duct system - closed dampers, closed registers, dirty filters, clogged coils
- Obstructions in the fan inlet - elbows too close to the inlet, walls too close to the inlet
- Duct design - improperly designed turning vanes, leaks in supply or exhaust ducts
- Fan related - impeller running backwards, fan speed too low, impeller dirty or clogged, clearances between inlet cone and wheel cone are incorrect
faqcategories :
- Roof Mounted Fans FAQs