Changing the Narrative: From Indoor Air Quality to Indoor Air Safety

by Mike Wolf, P.E. |

Before the pandemic, the majority of us took for granted that the air we breathe indoors is safe, just as we trust the water we drink is safe. Since the pandemic, we’ve learned that this is not always the case. Indoor Air Quality (IAQ) suddenly became a hot topic due to airborne viral transmission, especially since we spend 90% of our time indoors. However, IAQ covers several air-related issues including carbon dioxide (CO2) levels, Particulate Matter (PM) levels, Volatile Organic Compound (VOC) levels, and pathogen levels. In addressing these issues, the conversation has pivoted from Indoor Air Quality to Indoor Air Safety (IAS) and what we can do to mitigate these issues to create healthier indoor environments.

 

Foundational Air Safety Technologies

While IAS can be a complex issue, foundational HVAC technologies have been used for years and are proven to maximize indoor air quality and assure indoor air safety. These foundational technologies include: 

  • ventilation with outdoor air (OA), 
  • proper humidification, 
  • and air filtration.

 

Additive technologies have also become part of the IAS conversation, but these should be considered as part of a layered approach to enhance proven foundational technologies, not as an alternative to foundational technologies. Additive technologies include ionization (e.g., bipolar ionization, needlepoint bipolar ionization), dry hydrogen peroxide, ultraviolet germicidal irradiation, and carbon filtration. Some additive technologies can have unwanted and unsafe side effects such as ozone generation, increased concentration of VOCs, etc. When using additive technologies, especially to mitigate the risk of pathogens, it is imperative to verify the effectiveness of the technology through independent clinical studies that simulate real-life applications and equipment performance verification by third-party listing agencies.

 

Indoor Air Safety Strategies/Effectiveness

To assure the maximum impact on Indoor Air Safety it is critical to monitor the specific air safety issue being targeted and implement the HVAC technology that will provide the best solution for maintaining safety levels in the space (Figure 1).

 

 

Greenheck - IAQ Index

Figure 1: Source: https://greenecon.net/3-metrics-to-guide-air-quality-health-safety/carbon-footprint.html

 

Carbon Dioxide (CO2)

The level of carbon dioxide in the air is one of the most important metrics of Indoor Air Safety. CO2 is a reliable proxy for pathogen concentrations and is a simple compound to measure to monitor indoor air safety. Outdoor Air (OA) Ventilation is a proven and effective solution to reduce indoor CO2 levels.

 

Particulate Matter (PM)

Removing particulate matter (PM) from indoor air reduces the potential for spreading airborne pathogens. Many pathogens such as COVID cling to airborne particulate matter. As a result, reducing PM levels will also reduce the spread of airborne pathogens. Filtration and effective air distribution are proven solutions for removing particulate matter. Using efficient filters (MERV 13 or higher) along with an effective air distribution system that disperses air evenly throughout the space and circulates air to the filter system is an effective way to reduce pathogen-carrying particulate matter.

 

Volatile Organic Compounds (VOCs)

Volatile Organic Compounds (VOCs) are simply just carbon compounds (excluding compounds such as carbon dioxide) that exist in a gaseous state at room temperature. VOCs have various toxicity levels, so it’s important to know what compounds are present in a space. Because there are no standard recommendations for acceptable levels of VOCs, acceptable VOC concentrations will need to be established on a case-by-case situation. Outdoor air ventilation is highly effective at controlling VOC levels. Carbon filtration is another technology that is effective at filtering out VOCs. Like PM, the effectiveness of carbon filtration is highly dependent on effective air distribution that will assure airborne VOCs pass over the carbon filter. Ventilation is also more reliable given the delicate nature of carbon filters and susceptibility to being easily damaged by airborne PM.

 

Pathogens

Pathogens tend to thrive indoors and are most effectively controlled with a combination of foundational HVAC technologies. Ventilation with OA is effective at maintaining CO2 levels and because CO2 is a reliable proxy for pathogens, ventilation is effective in mitigating the risk of pathogens. The ideal range of relative humidity (RH) for human comfort is the same range where pathogens are not prevalent (Figure 2).

 

Greenheck - Optimum Humidity Range for Human Comfort and Health

Figure 2: Optimum Humidity Range for Human Comfort and Health. Source: 2016 ASHRAE HVAC Systems and Equipment Handbook Chapter 22.

 

Maintaining comfortable humidity levels maximizes IAS by reducing the concentration of pathogens in a space. Efficient Filtration with effective air distribution will eliminate dead zones and assure contaminated air passes over filters that can reduce particulate matter carrying pathogens. In specific and limited applications, Dry Hydrogen Peroxide (DHP) and UVGI may be an additional layer of technology for reducing concentrations of pathogens.

 

Greenheck - Air Health / Safety Effectiveness

 

For more information on Greenheck products that can help deliver safer, healthier indoor air, click here or contact your local Greenheck representative .

Indoor Air Quality
Mike Wolf, P.E.
Mike Wolf, P.E.
Mike Wolf, P.E.
Mike Wolf, P.E., is Industry & Regulatory Relations Senior Director at Greenheck Group, with nearly 40 years of experience across engineering, sales, marketing, and executive leadership. He is a recognized industry leader in HVAC regulations and standards development, actively working with organizations such as ASHRAE, AMCA, and AHRI and contributing to U.S. DOE energy regulation initiatives.
Other Blog Topics