Topic: Dampers

What You Need to Know About Fire Ratings to Select the Correct Ceiling Radiation Damper

by Michael Bulzomi |

Selecting the correct ceiling radiation damper (firestop flap for our friends in Canada) requires a solid understanding of the testing and expected damper performance. This understanding guides the selection based on the protection needed and shows the importance of proper selection and installation of the damper assembly. However, the ratings associated with ceiling dampers can be confusing since it is possible to have ceiling radiation dampers approved for several applications depending on the installation.

 

Ratings:  Fire-Resistance versus Fire-Protection

What is the difference between a fire-protection rating and a fire-resistance rating? Many products that protect openings have a fire-protection rating. However, assemblies designed for walls, floors, and ceilings must have fire-resistance ratings, per the International Building Code (IBC), specifically in ASTM E 119: Standard Test Methods for Fire Tests of Building Construction Materials or ANSI/UL 263: Fire Tests of Building Construction and Materials. The tests look at heat transfer through the membrane elements protecting the frame and surface of structures to confirm the assembly meets the stated criteria. The testing ensures proper performance in minimizing or preventing the fire from spreading and reducing the likelihood of structural failure.

 

Stated another way, the purpose of wall or ceiling assemblies having a fire-resistance rating is to:


  • Support an applied structural load
  • Prevent the spread of hot gases or flames through the exposed wall/ceiling
  • Limit temperature rise on the unexposed side so combustible materials on the unexposed side do not ignite from increased radiant heat

 

Products having a fire-protection rating (in general) only limit flames and do not prevent an increase in temperature from passing through to the unexposed side. Based on this information, ceiling dampers in floor/ceiling or roof/ceiling assemblies must have a fire-resistance rating instead of a fire-protection rating.

 

Selecting Ceiling Dampers

Selection for ceiling dampers involves much more than finding one with the desired features. The process requires a thorough understanding of the floor/ceiling or roof/ceiling assembly design because ceilings, like the assemblies installed, have different fire ratings. For example, a UL 555C-rated ceiling damper can provide the desired protection for air inlet/outlet penetrations while having a three-hour fire-resistance rating (assuming proper installation in the correct application). The ceiling damper in this example eliminates using a hinged-plate damper or similar protection methods for the design shown in the UL Fire Resistance Directory.

 

Buildings of wood construction can also pose a challenge when selecting ceiling radiation dampers. Approvals for ceiling dampers in wood construction differ from those required for other structures. Knowledge and understanding of ANSI/UL 263 are a must. This standard defines the test criteria to evaluate all building elements, including floor/ceiling assemblies, for fire resistance.

 

Referencing the UL Fire Resistance Directory for Wood Construction

Floor/ceiling assemblies that meet the test criteria of ANSI/UL 263 earn a fire-resistance rating expressed in hours. A damper manufacturer frequently sponsors this testing to verify the individual components in the assembly function as intended, allowing the assembly to receive the appropriate rating. Underwriters Laboratory (UL) then issues a design number for the newly rated floor or ceiling assembly and publishes the listing in its Fire Resistance Directory. The listing includes a drawing of the assembly and a detailed construction description. Potential confusion can happen at this point. The individual components of the assembly contribute to the fire resistance rating. However, that rating applies only to the assembly when used in that specific construction application. The ceiling damper and other individual components do not necessarily carry a specific hourly fire rating.

 

Summarizing Fire Ratings and Ceiling Dampers

A fire protection or fire-resistance rating is assigned to assemblies protecting openings in a tested fire-rated assembly. The IBC provides a detailed explanation of these ratings as it applies to building elements, components, and assemblies using test procedures explained in ASTM E 119 and ANSI/UL 263. However, a fire protection rating for a ceiling damper with UL 555C or a fire damper with UL 555 certification does not automatically allow use on a floor or ceiling assembly. You can and should refer to the UL Fire Resistance Directory, but a better approach is contacting your local Greenheck representative.

Dampers
Michael Bulzomi
Michael Bulzomi
Michael Bulzomi
Michael Bulzomi is Product Manager for Greenheck commercial dampers. He earned his MBA from Dowling College and his Bachelors in Earth Science and Atmospheric Science from the State University at Albany in New York. A member of ASHRAE, NFPA, and AMCA, he is the current Chair of the AMCA Fire and Smoke Damper Committee.
Other Blog Topics