Experience Best-In-Class Product Selection with:

eCAPSeCAPS

Vari-Green Constant Pressure Control

The Constant Pressure control is quite versatile and can be used to monitor either the static pressure or velocity pressure in a system. The control will automatically adjust the fan speed to maintain a desired static pressure or velocity pressure (used for constant CFM) in the system. This control will reduce energy consumption not only by reducing the speed and the energy used by the fan, but will also reduce the amount of conditioned air that is exhausted.