Project Profile: Wausau Curling Club
The Challenge
• Meet demand for large quantities of outdoor air to satisfy diverse load requirements
• Install a cost-effective air handling system that heats and cools the hospitality and viewing areas
• Minimize energy costs with energy recovery technology
• Control temperature to prevent fogging of glass between warmed hospitality area and much colder competition area
• Exhaust smoke, grease and odors from an open kitchen area
The sport of curling is a strategic game like chess, with an element of skill and experience. Played on ice in an indoor controlled environment, temperature and humidity are critical to setting ice speed and the amount of “curl” the stone will incur. Another design challenge was dealing with the variable loads without over-ventilating which would lead to extremely high utility bills.
The sport was invented in the early 16th century in Scotland. Today, curling is an Olympic sport for the very best and played by high school youth to senior adults.
In Wausau, Wisconsin, members of the local non-profit curling club were thrilled to open their new $5.2 million state-of-the-art curling center in late 2012. The new facility is among the largest and most technologically advanced curling centers in North America, and can accommodate up to eight games simultaneously.
Greenheck’s Solution
• (2) Energy Recovery Ventilators, Model ERV
• (2) Rooftop Ventilators, Model RV
• (2) Make-Up Air Unit, Model IGX
• (2) Exhaust Only Kitchen Hoods with Fire Suppression System
• (1) Canopy Type II Kitchen Hood
• (6) Louvers, Model ESD
• (12) Commercial Control Dampers
A large viewing and hospitality area with a working kitchen surrounds the curling competition area and needed to be efficiently heated, cooled and ventilated for post-competition parties and other activities. On most days, The Curling Center has few occupants. However, when a curling competition takes place, hundreds of competitors and spectators may gather in the hospitality and viewing areas. Large amounts of outdoor air are required for these diverse loads.
Since the all-volunteer, nonprofit Wausau Curling Club has no paid maintenance staff and uses the building mostly on a seasonal basis from October through April, a cost-effective, energy-efficient, dependable, and easy-to-operate ventilation system was imperative. Most of the ventilation equipment was installed outside at ground level to eliminate rooftop maintenance. Two, pre-engineered, energy recovery ventilators, Model ERV, with total enthalpy wheels were installed to handle exhaust air from the rest rooms while recovering energy from the exhaust air stream to precondition the ventilation air and reduce heating and cooling energy requirements. The makeup air units, Model IGX, with indirect fired-gas heating feature an 80% efficient furnace and heating capacities up to 1,200,000 BTU/hr (input). Supply airflow of up to 9,500 cfm and 3 inches of external static pressure help meet peak demand loads when the hospitality and viewing areas are filled to capacity. Two additional rooftop ventilators, Model RV, were installed to efficiently deliver and condition the appropriate mixture of outdoor and return air to the viewing space and hospitality areas.
Two exhaust only kitchen hoods with fire suppression systems handle grilling and other cooking tasks. A Canopy Type II kitchen hood (Model GD2) with single baffle was installed above the dishwasher to exhaust moderate condensation.
Model ESD louvers were installed in the exterior walls to protect air intake and exhaust openings in the building and minimize water penetration. Drain gutters are located on every blade to capture water which is dispersed to the jambs and drained out of the sill.