Search Results
Number of Results: 101
-
Louver Fundamentals: Understanding Louver Performance Criteria
The proper selection of louvers can be complex as many variables determine how they will perform. An understanding of basic louver performance criteria including free area, air volume, the beginning point of water penetration, and pressure drop can help guide your louver selection process. These per
-
EC Motor Fundamentals: Choosing the Right Motor—EC versus Belt Drive
New developments in EC motor technology and a growing list of benefits make EC motors attractive options in fan applications. But do these benefits make traditional belt drives obsolete? Let’s consider why customers select EC motors. All motors in fan equipment have two magnetic fields located in th
-
Louver Fundamentals: Form Meets Function
What exactly is a louver? What is its function in a building and an HVAC system? Simply, a louver is a device comprised of blades that permit the flow of air but inhibits the entrance of water or other elements. But simple doesn’t truly get at the form and function of louvers. Selecting the correct
-
HVAC Energy Recovery Technologies: Wheel versus Core
Energy recovery technology is commonly used in industrial, commercial, and institutional applications to provide comfort ventilation. Utilizing energy recovery allows for the supply airstream to be pre-conditioned by the return airstream, effectively reducing the amount of mechanical cooling or heat
-
Effective Strategies for Healthier Indoor Air
The importance of indoor air quality (IAQ) has continued to grow as we focus on improving societal health. Of course, the COVID pandemic has reinforced the need for well-designed ventilation systems that provide improved IAQ. If you are focused on improvement, particularly by reducing the efficacy o
-
Podcast: Amplifying UV-C performance for better IAQ
Newsmaker’s Coverage of AMPLIFY™ Overhead fans with Northern Light® Technology Listen as Tyson Sargent, segment manager for Greenheck’s overhead HVLS products, shares valuable information on AMPLIFY™ overhead fans with Northern Light® technology. Once you've listened to the podcast, read more about
-
Leverage Employee Comfort and Make it a Critical Part of Your Hiring Strategy
“How do I attract and retain employees for my distribution centers?” That’s a great question because the warehousing and storage market segment is growing exponentially. From 2010 through projections for 2022, CAGR for the Warehouse segment have come back at nearly 25% (Dodge Data & Analytics) with
-
A healthier, more comfortable, environment for employees and plants.
A typical outdoor greenhouse can reach 110ºF inside making conditions uncomfortably warm and humid especially during summer months. Air movement is critical to lowering the temperature as well as moisture evaporation to help keep plants healthier.
-
3 Reasons to Work with a Greenheck Rep
Many in the HVAC industry have a go-to-market model using manufacturer’s representatives as the sales force. Finding every niche in a geographical market requires a large sales team, more than most companies can afford. The manufacturer’s reps provide tremendous value to customers in their local mar
-
Exhaust System Stack Design and Plume Rise
One of the critical features of a properly designed laboratory or industrial exhaust system is the exhaust stack. The exhaust stack helps ensure polluted exhaust is dispersed into the atmosphere before it can be re-entrained into building air intakes or settle on occupied areas such as building entr
-
5 Ways to Create and Maintain Perfect Building Temperature Using the Right Equipment
If you've ever worked when it's too hot or too cold, concentrating, being productive, and getting the job done is tough. Sweat dripping into your eyes or tensed up muscles from the chill can make life exponentially harder. That’s why maintaining a relatively stable and comfortable temperature is so
-
Fans vs. Air Conditioners: Which Cools Better?
Keeping an indoor space at a comfortable temperature is extraordinarily important. There are many options available to accomplish that task, and some are far better than others. The two basic methods are fans and air conditioners but figuring out exactly which works best for your particular situatio
-
Three Tactics to Improve Indoor Air Quality (IAQ) in Schools and Commercial Buildings
The COVID-19 pandemic has opened the eyes of many regarding the importance of indoor air quality (IAQ) in schools and commercial buildings. Poor IAQ causes illness and other health problems. The impact of poor IAQ becomes worse when you consider this key statistic: The Environmental Protection Agenc
-
How to Cool a Building Without Air Conditioning
When the weather warms up, an air conditioning unit can help keep large indoor spaces comfortable. But sometimes installing an air conditioning unit isn’t always possible or economical, so finding ways to cool the interior of a building without using AC is necessary. There are numerous benefits to k
-
How to Avoid the High-Temperature (and Odorous) Exhaust Associated with Diesel Generators
Electricity. Practically everyone uses it. We power everything from a children's toy to hearing aids using some form of electrical power. Electric power makes life productive and comfortable. Sometimes, it even saves lives. However, what happens when the power is interrupted? For most, it's an irrit
-
Provide correct air changes to laboratory, office and warehouse.
Providing a 100% outdoor air ventilation solution can be challenging when a rooftop installation will not work. Learn how Greenheck’s solution allowed for the installation of dedicated outdoor air systems units without costly plenum curbs.
-
Dollar Per CFM - Why is it Important
Many options exist for building ventilation. Most options depend on the building’s use. For example, warehouses, distribution centers, and manufacturing buildings often use a combination of gravity and powered fan equipment to ventilate the facility. This method is popular because it offers effectiv
-
When is Make-Up Air Required for Kitchens?
When is Make-Up Air Required for Kitchens? Have you ever left a restaurant smelling like you’ve been cooking burgers for hours? If you have, it could be that the restaurant has a make-up air/exhaust system not working correctly. Selecting the correct make-up air solution for your kitchen can be the
-
Why is My Bathroom Mirror Foggy?
Bath Fans and the Importance of Certified Airflow Should a company manufacture products that perform as tested in ideal conditions or conditions based on real-life experiences? This conundrum is an age-old debate. For example, would you buy a new vehicle that advertised its fuel efficiency based on
-
Energy Efficiency and Indoor Air Quality Help Transform 94-Year-Old Building
Older buildings have many qualities, such as architectural features not seen on many newer structures. However, few have the energy efficiency required to attract tenants. Learn how Greenheck’s solution improved energy efficiency and indoor air quality (IAQ).
-
How to Select the Best Kitchen Hood for a Residential Kitchen in a Commercial Building
Selecting a kitchen hood is a relatively straightforward decision for a restaurant or commercial kitchen. The decision is equally straightforward when purchasing a kitchen hood for your house. One simply selects the features needed and desired that meet the various building codes for the location an
-
Be Confident In Your HVLS Fan Selections
High volume, low speed (HVLS) fans are large diameter ceiling fans that circulate large volumes of air at low operational speeds. These fans are increasingly popular because of two main uses-- thermal comfort and energy efficiency. Several companies currently manufacture HVLS fans, providing end-use
-
Sign-Up for and Comment on Fresh Air Blog Posts
Greenheck’s Fresh Air blog recently added new functionality to make your blog experience even better. Now, you can have notifications of new blog posts sent directly to your email inbox. We know your time is valuable and this notification can save you time. But that’s not all. Our intention has alwa
-
What You Need to Know About DOAS And the New Efficiency Ratings
Dedicated outdoor air systems (DOAS) are gaining popularity in the commercial HVAC industry. These systems consist of ventilation units that dehumidify 100% outdoor air coupled with air handling units that heat or cool the space air. Figure 1 is a schematic of a typical DOAS. Figure 1: DOAS units pr
-
How to Adjust Your HVAC System and Minimize the Spread of COVID-19
Keeping people safe and protected from contagious viruses has reached unprecedented levels over the past few months. Leading organizations such as the Center for Disease Control (CDC) and medical professionals stress the need for common sense practices to slow the spread of COVID-19 and other contag
-
How to Select the Proper Explosion-Proof Motor for Your Fan Application
A variety of exhaust fans with spark-resistant designs that are suitable for contaminated and flammable environments are available in the marketplace. Many of these environments can use totally enclosed (TE) motors since the motors are not in the contaminated airstream and pose no threat to ignite a
-
Understanding the basic Operation of a Variable Volume Lab Exhaust System
Lab ventilation systems are traditionally high users of energy based on the objectives of: Safely exhausting fumes and odors from the lab space Expelling fume and odor contaminants above the facility to prevent entrainment back into the lab or neighboring facilities Supplying 100% fresh make-up air
-
Understanding FEI; the new Fan Energy Index
As the saying goes “The only thing that is constant is change.” As we all know, change isn’t always good. However in this case, changing to the new Fan Energy Index (FEI), replacing the much criticized and flawed FEG (Fan Efficiency Grade) metric, is great! FEI replaces existing fan energy metrics i
-
Elements of motor sizing
What size motor best suits a fan? It is a common question that is more complex than one would imagine. Many variables exist based on an application. Different technologies also affect the fan selection. The following will discuss torque, horsepower and fan laws. Here is an example. “My direct drive
-
Considerations for Warehouse Summer Ventilation Systems
Heat builds up in warehouses and distribution centers in the summer months without proper ventilation. Summer ventilation systems exhaust heated air from the warehouse and replaces it with fresh outdoor air. These systems replace the air in the building 1 – 3 times per hour, which minimizes the diff
-
How Well do You know Your Industrial Isolation Dampers?
Dampers can have many different functions within an HVAC or process application. One such function prevents or restricts the free flow of air, requiring the use of an isolation damper. Isolation dampers are generally two-position dampers and actuated to be fully open or fully closed. The degree of i
-
How to Avoid Selecting the Wrong Ceiling Damper
Ceiling dampers, also called ceiling radiation dampers (Figure 1), are crucial components of fire-rated floor/ceiling and roof/ceiling assemblies. However, confusion often occurs during the specifying and selection of these products. It is common to install the wrong damper, or worse, install each i
-
Fresh Air for the HVAC Industry
Welcome to the blog for air movement, control, and conditioning professionals that addresses your technical interests and needs. You will find valuable information on topics important to you and your work as it relates to heating, ventilation, and air conditioning (HVAC). No hype or hyperbole—just v
-
Leading Causes of Coil Failures Explained
Whether you own a large commercial building or are homeowner, you rely on heating, ventilation and air conditioning (HVAC) equipment to maintain the comfort level of your building. While this equipment is reliable, it inevitably fails. Then, if you find the culprit is a heating or cooling coil, you
-
Understand the Energy Efficiency Codes Before Selecting an Inline Fan
Are you in the market for an inline fan? Wonderful! Many energy-efficient options exist. But how do you know whether the inline fan you select offers the performance you want and complies with relevant codes and standards? Perhaps a better question is, do you know what codes and standards emphasize
-
Exploring the Benefits of Factory-Installed Ceiling Radiation Damper—Bath Exhaust Fan Combination
Bathroom exhaust fans are the most common way to properly ventilate and control moisture in residential bathrooms. Along with providing effective ventilation, bath fans with a ceiling radiation damper (CRD) are one of many components used to mitigate the spread of fire in many multi-family residenti
-
Louver Requirements for the Hurricane-Prone Region
Nearly 40 hurricanes and tropical storms have made landfall in the United States (U.S.) and its territories in the past 10 years. These storms pose an extreme risk for inhabitants of the areas affected. This risk includes injury and loss of life. Risk also extends to damage incurred to property—home
-
How to Survive a Retrofit Fan Installation in a Tight Space Location
Specifying and installing a [physically] large fan and its related housing in new construction frequently is quite easy. Exposed openings allow contractors to move it to the required location. However, that same installation to replace the existing equipment becomes far more difficult years after th
-
Aspirus Wausau Hospital Medical Surgical ICU Remodeling
The intensive care unit of a hospital requires a unique approach to ventilation to protect against contaminated air and pathogens, and still maintain patient comfort. Learn how Greenheck provided the right solution.
-
Apply energy recovery to ventilation systems -- It's the Law!
Recovering energy sounds pretty good, right? But how many realize it is possible to recover energy from HVAC equipment that is ventilating a space? An energy recovery ventilator (ERV) consists of a supply fan, exhaust fan, and an energy recovery device. The ERV takes spent/stale conditioned air from
-
Improved Indoor Air Quality Raises Math/Science Scores
tbd Indoor air quality is a concern in schools across the country. It affects health and the ability to learn. Yuma High School in Yuma, Arizona solved its air quality challenge and eliminated another common issue. Read about Greenheck’s solution.
-
The Impact of Poor Indoor Air Quality in Multifamily Buildings
According to the United States Environmental Protection Agency (EPA), the concentration of some pollutants is often 2 to 5 times higher indoors than outdoors. The average American spends approximately 90% of their time indoors, so indoor air quality (IAQ) is extremely important to everyone’s health.
-
How to Adjust Air Performance in the Field without Sheave Changes or VFDs on Adjustable Blade Fans
Air performance adjustments in the field are sometimes necessary for a variety of reasons. For example, the system’s design looks perfect on paper, but the realities of installation can require airflow changes. Other factors include unaccounted or overestimated pressures, or building renovations. It
-
Fire Dampers 101 – Types, Testing, and Ratings
Fire dampers play a very important role in protecting buildings and saving lives in the event of a fire. Building codes require fire dampers to maintain the fire-resistance ratings of walls, partitions, and floors when penetrated by air ducts and transfer openings. (Figure 1) Upon detection of eleva
-
The Energy Savings Revolution in Make-up Air
A mechanical ventilation system provides fresh, outdoor air, as well as heating and cooling to the space in most commercial buildings. The system design varies depending on the application and uses various components such as air-handlers, make-up air units, and energy-recovery ventilators. Each prod
-
Does Your HVLS Fan Perform As Advertised?
High volume, low speed (HVLS) fans are large diameter ceiling fans that have gained significant popularity in the HVAC industry over the last several years. Like your ceiling fan at home, HVLS fans are a great way to circulate air and make the places that we live and work more comfortable. But, unli
-
Understanding LODs and its Use in Building Information Modeling
Building information modeling (BIM) in its most simplistic form is all about data; specifically, the data contained in individual BIM elements. These elements – e.g., walls, windows, doors, fixtures, etc. – are the building blocks of any building information model, and can each contain information t
-
Improved Thermal Comfort and Aesthetics Make the Journey Enjoyable
TBD Central Wisconsin Airport in Mosinee, Wisconsin serves as a gateway for leisure and business travel. More than 280,000 people use the airport annually. Read about Greenheck’s solution to improve thermal comfort with using stylish fans that complements the airport’s newly remodeled concourse.
-
How to Design Laboratory Ventilation
The COVID-19 pandemic exposed the need for more information in fighting contagious diseases. Research on its causes, controls and cures spiked and continue still as the world attempts to protect against such viruses. Of course, laboratories work on a variety of projects in addition to contagious dis
-
Protecting Ventilation Openings for Storm Shelters and Tornado Safe Rooms; FEMA Louver Requirements
Springtime in many parts of North America ushers in many changes. Snow melts, temperatures rise and the land starts producing again. These are welcome changes for many, but these changes do not come without some challenges. Spring is a volatile season and is often known for violent weather. Tornadoe