Ceiling Exhaust Fans FAQQA1
Do you have two-speed (whole house/continuous ventilation) fans?
Link text :
Select a Card/Question Answer :
QuestionAnswer
Display order :
1
Yes. Our "whole house ventilation" option is our two speed offering. When this option is selected, the fan will run continuously at the user defined low speed (set by speed controller) and ramp up to the certified airflow rate on demand. Several switch options allow the fan to run at high speed including wall switch, motion detector, humidity sensor, etc. as wired by the electrician.
faqcategories :
- Ceiling Exhaust Fans FAQs
Related pages :
from