CAPS® 4.48
Canada and International
Air Movement Products - Rep Partner CAPS (CA)
*Quick Build options are now available on BAER belt drive sidewall fans (all propeller types and sizes) and AER direct drive sidewall fans with steel propellers (sizes 20 through 48)
Video: CAPS v4.48 Training - Ceiling
*Select by manufacturer option (listed on the model tab)
-Four bath fan competitors were added: Panasonic, Broan, DeltaBreez, and Loren Cook
-Cross-referenced to equivalent Greenheck models
*Not Preferred Flag
-Populates with select options that might not be ideal or competitive with large, multifamily jobs
-Galvanized wheel is an example
Video: CAPS v4.48 Training - CVI
*USF is moving to the new user interface to match many of the other fan models
*USF belt drive sizes 27 and larger have transitioned to the Gen 2 design, which uses the A2 and B6 wheels
*Added new center of gravity drawings for model USF
*Add shipped loose VFDs, available up to 30 hp (models USF and AP family)
*Obsoleted the VFD Control Package on the USF
Video: CAPS v4.48 Training - Inlines
*Quick Build improvements
-RSQ size 7-24 now QB15
-KSQ size 18-24 now QB10
-SQ Mixed Flow side discharge now QB5, filter section & baffle now QB10
*Expanded VG motor options (1/10, 1/6, 1/3, 3/4 hp now available)
*KSQ & RSQ now have the M1 option for a composite wheel
*"High wind rated" option for SQ Outdoor, KSQ, RSQ has officially received NOA from Miami-Dade
*No new selections on model LB / RSF. Please see model RSQ
*No changes
*Northern Light HVLS models DC-5-7-NL, DC-5-10-NL, DC-5-14-NL, and DC-5-16-NL are no longer selectable in the CAPS 4.48 release. Orders for existing marks will be accepted until December 2025 (CAPS 4.49 release). All other DC-5 models will continue to be available
Video: CAPS v4.48 Training - PRV
*Generation 2 for upblast continues to be implemented
-Multiple conduit chases can now be selected (0, 1, and 2)
-Expanded multiple curb cap sizes up to size 160
*There will be two HOAs available for Vari-Green selections. The HOA ‘Ship Loose’, which has been there for several releases, and now the ‘HOA w/Enclosure’. This is a pre-mounted HOA in a 12x12x8 NEMA 3R enclosure
*Model AX 100 Series is available on QD/Stock program
Air Movement Products - Rep Partner CAPS 4.48 (Intl)
*Quick Build options are now available on BAER belt drive sidewall fans (all propeller types and sizes) and AER direct drive sidewall fans with steel propellers (sizes 20 through 48)
Video: CAPS v4.48 Training - Ceiling
*Select by manufacturer option (listed on the model tab)
-Four bath fan competitors were added: Panasonic, Broan, DeltaBreez, and Loren Cook
-Cross-referenced to equivalent Greenheck models
*Not Preferred Flag
-Populates with select options that might not be ideal or competitive with large, multifamily jobs
-Galvanized wheel is an example
Video: CAPS v4.48 Training - CVI
*Obsoleted the VFD Control Package on the USF
Video: CAPS v4.48 Training - Inlines
-SQ Mixed Flow side discharge now QB5, filter section & baffle now QB10
*No new selections on model LB / RSF. Please see model RSQ*Models SQ, KSQ, and RSQ are now available with the ACH-580 variable frequency drive (VFD) (60 cycle only)
*No changes
*Northern Light HVLS models DC-5-7-NL, DC-5-10-NL, DC-5-14-NL, and DC-5-16-NL are no longer selectable in the CAPS 4.48 release. Orders for existing marks will be accepted until December 2025 (CAPS 4.49 release). All other DC-5 models will continue to be available
Video: CAPS v4.48 Training - PRV
*Generation 2 for upblast continues to be implemented
-Multiple conduit chases can now be selected (0, 1, and 2)
-Expanded multiple curb cap sizes up to size 160
*There will be two HOAs available for Vari-Green selections. The HOA ‘Ship Loose’, which has been there for several releases, and now the ‘HOA w/Enclosure’. This is a pre-mounted HOA in a 12x12x8 NEMA 3R enclosure
*Model AX 100 Series is available on QD/Stock program
Conditioning and Ventilating Products - Rep Partner CAPS (CA)
Video: CAPS v4.48 Training - RTU
*New RT-40/70/120 all available for selections and ordering – click here for more info
-6.5-30 tons of PDX cooling
-10-30 tons of ASHP (6.5-10 tons ASHP coming soon)
-65kA SCCR option
-Backup or Supplemental Heat will be available on ASHP selections
-Curbs for all housings
-Coil Coating options
-Kitchen Controls
*Coming soon!
-RT-40 6.5-10 tons ASHP – December 2025
-RT-20 3-5 tons PDX and ASHP – April 2026
Video: CAPS v4.48 Training - DOAS
*New RV-220 Housing: Now supports up to 100 tons of cooling and airflow up to 29,200 cfm
*Quick Build Program: Predetermined configuration options qualify for 15, 20, or 25-day Quick Builds with a price premium
*DOAS Nomenclature: Model names updated to align with current energy recovery models. For example, RV-25 will become RV-40 in CAPS 4.48
*Energy Recovery: Improved accuracy in energy recovery calculations
*Partial Recirculation with PDX: Restrictions apply to selected housings
Video: CAPS v4.48 Training - ERV
*Model ERM has been discontinued
Video: CAPS v4.48 Training - KVS
*New fire ready basic residential range hood, model GRRB - available for selections and quotes
*Jobs located outside the continental United States will only be selectable with pre-pipe only fire suppression systems
*Advanced controls bug fixes (advanced system overview report, sump wash only, and wash cabinet height)
*New PCB controls version V5 firmware update
*Fixed Greenheck quotation bug with MS Word (related to fire field hookup pricing)
Video: CAPS v4.48 Training - MUA
*New PDX for H22 housing in models DGX/MSX
-Airflow ranges up to 9,000 cfm
-7, 10, 16 ton cooling capacities
-PDX performance values are subject to change in the next update coming in December
*Launched new user interface for models: DGX, TSU, VSU, GREENHEAT, IGX, MSX, TSF, KSQ
*Obsolescence of the terminal strip and remote panel control offerings (previously saved selection will convert to microprocessor control)
*Obsolescence of both hot water and steam face and bypass coil offerings (previously saved selections will have these options removed and will have to be reselected)
Conditioning and Ventilating Products - Rep Partner CAPS 4.48 (Intl)
Video: CAPS v4.48 Training - DOAS
*Partial Recirculation with PDX: Restrictions apply to selected housings
Video: CAPS v4.48 Training - ERV
*New model IVE is orderable
*2 hp single-phase motor added for ERVi and IVE
*Quick Builds disabled for ERV-90 & ERV-120
*Hi-Pro Poly Coatings have been discontinued on all ERV products
*Model ERM has been discontinued
Video: CAPS v4.48 Training - KVS
*New fire ready basic residential range hood, model GRRB - available for selections and quotes
*Jobs located outside the continental United States will only be selectable with pre-pipe only fire suppression systems
*Advanced controls bug fixes (advanced system overview report, sump wash only, and wash cabinet height)
*New PCB controls version V5 firmware update
*Fixed Greenheck quotation bug with MS Word (related to fire field hookup pricing)
Video: CAPS v4.48 Training - MUA
*New PDX for H22 housing in models DGX/MSX
-Airflow ranges up to 9,000 cfm
-7, 10, 16 ton cooling capacities
-PDX performance values are subject to change in the next update coming in December
*Launched new user interface for models: DGX, TSU, VSU, GREENHEAT, IGX, MSX, TSF, KSQ
*Obsolescence of the terminal strip and remote panel control offerings (previously saved selection will convert to microprocessor control)
*Obsolescence of both hot water and steam face and bypass coil offerings (previously saved selections will have these options removed and will have to be reselected)
Air Control Products- Rep Partner CAPS (CA)
Video: CAPS v4.48 Training - Dampers
*Obsoleted platform for heavy-duty/industrial control, rectangular isolation, and round backdraft product families (final release to place orders using the obsoleted platform)
*Models KFD-150, KFD-350, CRD-1LP, CRD-60X are no longer available for selection
*Models SSFSD-211, SSSMD-201, and SMD-302M are no longer available for order
*“Damper Labels” accessories are no longer available for order
*Pressure drop performance data is now available for curtain fire dampers
*Siemens GJD/GRD series actuators are available for 24 VDC actuator type on volume control dampers
*Honeywell MSxx20 series actuators are available for volume control dampers
*Updated CAPS drawings for DFD and FD X-Series dampers
*Various help text updates
*Lead time updates for various heavy-duty models and selections
*Quick Build maximum dollar limits updated for heavy-duty dampers
*Maximum size reduction for HCD-240 and HB-240 selected with spark A resistance
*For a complete list of details click here
Video: CAPS v4.48 Training - Louvers
*Only rectangular shapes will be selectable for all “X” models. Shape options are no longer selectable on ESD-435X, ESD-635X, and EHH-501X
-Shapes are still allowable, but only as SDRs
*Galvanized or Galvanneal material no longer selectable on acoustical louver models AFJ-601, AFJ-801, and AFJ-120
*New flanged/sleeve (anchorless) installation available for model EVH-501D
*Total concession of minimum finish charge on the seven (7) most popular standard colors (Bone White, Classic Bronze, Clear Anodize Mica, Stone Gray, Flat Black, Spartan Bronze, and Dove Gray) when AAMA 2605 2-coat or 3-coat 70% Kynar/100% Fluoropolymer is selected
Air Control Products -Rep Partner CAPS 4.48 (Intl)
Video: CAPS v4.48 Training - Dampers
*Obsoleted platform for heavy-duty/industrial control, rectangular isolation, and round backdraft product families (final release to place orders using the obsoleted platform)
*Models KFD-150, KFD-350, CRD-1LP, CRD-60X are no longer available for selection
*Models SSFSD-211, SSSMD-201, and SMD-302M are no longer available for order
*“Damper Labels” accessories are no longer available for order
*Pressure drop performance data is now available for curtain fire dampers
*Siemens GJD/GRD series actuators are available for 24 VDC actuator type on volume control dampers
*Honeywell MSxx20 series actuators are available for volume control dampers
*Updated CAPS drawings for DFD and FD X-Series dampers
*Various help text updates
*Lead time updates for various heavy-duty models and selections
*Quick Build maximum dollar limits updated for heavy-duty dampers
*Maximum size reduction for HCD-240 and HB-240 selected with spark A resistance
*For a complete list of details click here
Video: CAPS v4.48 Training - Louvers
-Shapes are still allowable, but only as SDRs
*Galvanized or Galvanneal material no longer selectable on acoustical louver models AFJ-601, AFJ-801, and AFJ-120
*New flanged/sleeve (anchorless) installation available for model EVH-501D
*Total concession of minimum finish charge on the seven (7) most popular standard colors (Bone White, Classic Bronze, Clear Anodize Mica, Stone Gray, Flat Black, Spartan Bronze, and Dove Gray) when AAMA 2605 2-coat or 3-coat 70% Kynar/100% Fluoropolymer is selected
CAPS® 4.47
Canada and International
Air Movement Products - Rep Partner CAPS 4.47 (Intl)
Model AER and BAER transitioned to the new fan user interface with selection speed and functionality improvements
Video: CAPS v4.47 Training - Ceiling
Model SP and CSP transitioned to the new fan user interface with functionality improvements
SP-LP Contractor packs available for all variations
Mounted Ceiling Radiation Dampers (CRDs) available for SP-LP models (SP-LP0511H/HL and SP-LP0810W/WL)
Video: CAPS v4.47 Training - Centrifugal
New model FJ (combination of redesigned FJI and current FJC) to use the new fan user interface with selection speed and functionality improvements
FJI is being discontinued, but still available as a legacy product selection as *FJI
The FJC with the old user interface is available via the *FJC for a release
Stopped accepting orders for USF-B2/B3 (USF-B7 replaces any prior selections)
Video: CAPS v4.47 Training - Inline
Direct drive inline model SQ:
Price reduction on all sizes
New, low-cost size 12-M1 with composite wheel
Improved QB programs on standard construction units and accessories
Roof-mounted supply model KSQ:
Price reduction on base fan and weatherhood – all sizes
Improved QB programs on standard construction units and accessories
Sizes 27 through 33 ship assembled from the factory (previously only 7 through 24 shipped assembled)
Roof exhaust and roof supply model RSQ:
Price reduction on base fan and hood (excluding aluminum hood) – all sizes
Initiation of RSQ QB program
No changes
No changes
New pricing category FV9
FV1 = upblast and downblast (CUE/G) sizes 240 and smaller
FV7 = upblast and downblast (CUBE/GB) sizes 240 and smaller
FV9 = upblast and downblast (CUE/CUBE and G/GB) sizes 260 and larger
New 2.5-inch thick insulation option (R10 value) on all insulated PRV curb models
Curb Extensions (GPE, GPEX, ISB, VCE, ATE) moved to use the new user interface
Model USGF is being removed from legacy CAPS
For the AX/QEID (direct drive FETI models) the VFD accessory no longer defaults “On” when selecting using a VFD
Price reduction on AX 100 series fans. These are stocked products
Air Movement Products - Rep Partner CAPS 4.47 (CA)
Model AER and BAER transitioned to the new fan user interface with selection speed and functionality improvements
Video: CAPS v4.47 Training - Ceiling
Model SP and CSP transitioned to the new fan user interface with functionality improvements
SP-LP Contractor packs available for all variations
Mounted Ceiling Radiation Dampers (CRDs) available for SP-LP models (SP-LP0511H/HL and SP-LP0810W/WL)
Video: CAPS v4.47 Training - Centrifugal
New model FJ (combination of redesigned FJI and current FJC) to use the new fan user interface with selection speed and functionality improvements
FJI is being discontinued, but still available as a legacy product selection as *FJI
The FJC with the old user interface is available via the *FJC for a release
Stopped accepting orders for USF-B2/B3 (USF-B7 replaces any prior selections)
Video: CAPS v4.47 Training - Inline
Direct drive inline model SQ:
Price reduction on all sizes
New, low-cost size 12-M1 with composite wheel
Improved QB programs on standard construction units and accessories
Roof-mounted supply model KSQ:
Price reduction on base fan and weatherhood – all sizes
Improved QB programs on standard construction units and accessories
Sizes 27 through 33 ship assembled from the factory (previously only 7 through 24 shipped assembled)
Roof exhaust and roof supply model RSQ:
Price reduction on base fan and hood (excluding aluminum hood) – all sizes
Initiation of RSQ QB program
No changes
No changes
New pricing category FV9
FV1 = upblast and downblast (CUE/G) sizes 240 and smaller
FV7 = upblast and downblast (CUBE/GB) sizes 240 and smaller
FV9 = upblast and downblast (CUE/CUBE and G/GB) sizes 260 and larger
New 2.5-inch thick insulation option (R10 value) on all insulated PRV curb models
Curb Extensions (GPE, GPEX, ISB, VCE, ATE) moved to use the new user interface
Model USGF is being removed from legacy CAPS
For the AX/QEID (direct drive FETI models) the VFD accessory no longer defaults “On” when selecting using a VFD
Price reduction on AX 100 series fans. These are stocked products
Conditioning and Ventilating Products - Rep Partner CAPS 4.47 (Intl)
Video: CAPS v4.47 Training - DOAS
New user interface enhancements
65kA SCCR option
Increased supply air CFM and heating capacity for RV-45, RVE-85, and RVC-65
Video: CAPS v4.47 Training - ERV
ERVi Side Discharge configuration
New Indoor Ventilator with Energy Recovery model IVE
Integrated electric heat option
Selections only in April
Orderable in August
ECV Outdoor all end connections
Re-aligned ERV model tree
Video: CAPS v4.47 Training - KVS
Two new Pollution Control Units (PCU) with capacities up to 18,000 and 27,000 cfm respectively
Fans shipped separately
VFDs >25 hp shipped loose
New advanced controls configuration
Replaces ASCP and Melink® control packages
Allows for use of multiple UIs on a single GKC package
Amerex® pricing category added which allows for more detailed pricing as we move forward
Amerex® list prices reduced by roughly 5% due to cost savings discovered on fire system components
Green Line additions
Custom light quantities
18-inch diameter exhaust collars shipped loose
Fixed PCU submittal bugs
Amended skewed drawings
Updated filter information
Video: CAPS v4.47 Training - MUA
Additional fan model for PDX offering to meet upper limit airflows with some external static pressure
Standardized on stainless steel for our IGX heat exchanger material
Began controls simplification to remove the terminal strip and remote panel control offerings for make-up air models
Conditioning and Ventilating Products - Rep Partner CAPS 4.47 (CA)
Video: Greenheck RTU Product Introduction - March 2025
New Packaged Rooftop Units, models RT-70, RT-120, are available to make selections. For additional information click here
Video: CAPS v4.47 Training - DOAS
New user interface enhancements
65kA SCCR option
Increased supply air CFM and heating capacity for RV-45, RVE-85, and RVC-65
Video: CAPS v4.47 Training - ERV
ERVi Side Discharge configuration
New Indoor Ventilator with Energy Recovery model IVE
Integrated electric heat option
Selections only in April
Orderable in August
ECV Outdoor all end connections
Re-aligned ERV model tree
Video: CAPS v4.47 Training - KVS
Two new Pollution Control Units (PCU) with capacities up to 18,000 and 27,000 cfm respectively
Fans shipped separately
VFDs >25 hp shipped loose
New advanced controls configuration
Replaces ASCP and Melink® control packages
Allows for use of multiple UIs on a single GKC package
Amerex® pricing category added which allows for more detailed pricing as we move forward
Amerex® list prices reduced by roughly 5% due to cost savings discovered on fire system components
Green Line additions
Custom light quantities
18-inch diameter exhaust collars shipped loose
Fixed PCU submittal bugs
Amended skewed drawings
Updated filter information
Video: CAPS v4.47 Training - MUA
Additional fan model for PDX offering to meet upper limit airflows with some external static pressure
Standardized on stainless steel for our IGX heat exchanger material
Began controls simplification to remove the terminal strip and remote panel control offerings for make-up air models
Air Control Products - Rep Partner CAPS 4.47 (Intl)
Video: CAPS v4.47 Training - Dampers
Enhanced user interface for QD/Stock damper, accessories and parts
Automatic conversion to new user interface
Convenient Mark Info pop-up
Obsoleted user interface for access doors, automatic balancing, backdraft, ceiling radiation, and remote balancing product families
Discontinued models SSFSD-211; SSSMD-201; SMD-302M
Discontinued 304 SS frame material for VCD-34, 34V and 42 models
New stock product models MBDR-CBL
New Single Side Components option for smoke and combination fire smoke models
Video: Single Side Component Option - Multi-Blade Life Safety Dampers in CAPS
Updated component location drawings
Actuator running time for Siemens GJD series actuators
Restored .CSV file export for equipment schedules
Best available lead time updated to 10-Day for HPR-330 damper model
Best available lead time for heavy-duty/industrial damper with coatings previously available as 10-Day updated to 15-Day
Pressure settings for PRAD and VRAD models
Correction to width/height note on cut sheet and submittal reports for BD and WD models
Click here for additional damper details
Video: CAPS v4.47 Training - Louvers
Quick Build Refinement For Targeted Capacity - the following selections will no longer be available on a QB program (standard lead time only)
AAMA 2603 (Baked Enamel and Industrial Epoxy) and AAMA 2604 (Acroflur 50% Kynar and Hi-Pro Polyester)
Optional welded construction
Flange size “other”
1-inch mesh bird screen
Flat black bird screen
Triangular shapes
Obsolescence
New selections of the following models will no longer be available in CAPS 4.47. Prior selections still orderable up until CAPS 4.48.
EDD-601, ESK-402, EHM-601, EACC-401, GCE-402, AFA-801
0.125-inch blade for models ESD-403 and ESD-603 no longer available in CAPS 4.47. Prior selections will no longer be orderable
Environmental Product Declarations - 28 of our most popular louvers have downloadable documents as part of the submittal under the Damper/Louver section
Only those models that have an EPD will print an EPD when selected
Air Control Products- Rep Partner CAPS 4.47 (CA)
Video: CAPS v4.47 Training - Dampers
Enhanced user interface for QD/Stock damper, accessories and parts
Automatic conversion to new user interface
Convenient Mark Info pop-up
Obsoleted user interface for access doors, automatic balancing, backdraft, ceiling radiation, and remote balancing product families
Discontinued models SSFSD-211; SSSMD-201; SMD-302M
Discontinued 304 SS frame material for VCD-34, 34V and 42 models
New stock product models MBDR-CBL
New Single Side Components option for smoke and combination fire smoke models
Video: Single Side Component Option - Multi-Blade Life Safety Dampers in CAPS
Updated component location drawings
Actuator running time for Siemens GJD series actuators
Restored .CSV file export for equipment schedules
Best available lead time updated to 10-Day for HPR-330 damper model
Best available lead time for heavy-duty/industrial damper with coatings previously available as 10-Day updated to 15-Day
Pressure settings for PRAD and VRAD models
Correction to width/height note on cut sheet and submittal reports for BD and WD models
Click here for additional damper details
Video: CAPS v4.47 Training - Louvers
Quick Build Refinement For Targeted Capacity - the following selections will no longer be available on a QB program (standard lead time only)
AAMA 2603 (Baked Enamel and Industrial Epoxy) and AAMA 2604 (Acroflur 50% Kynar and Hi-Pro Polyester)
Optional welded construction
Flange size “other”
1-inch mesh bird screen
Flat black bird screen
Triangular shapes
Obsolescence
New selections of the following models will no longer be available in CAPS 4.47. Prior selections still orderable up until CAPS 4.48.
EDD-601, ESK-402, EHM-601, EACC-401, GCE-402, AFA-801
0.125-inch blade for models ESD-403 and ESD-603 no longer available in CAPS 4.47. Prior selections will no longer be orderable
Environmental Product Declarations - 28 of our most popular louvers have downloadable documents as part of the submittal under the Damper/Louver section
Only those models that have an EPD will print an EPD when selected
CAPS® 4.46
Canada and International
Air Movement Products - Rep Partner CAPS 4.46 (Canada + INTL)
*Hooded propeller and Fabra hoods have a new High Wind rating Notice of Acceptance number, NOA 23-1122.03
*Wall-mounted models AER and BAER fabricated steel propeller lead time updated from extended to standard (all sizes)
*No changes
▶️ Watch the Centrifugal Fans CAPS Training Video ▶️
*Plenum models APD, APH, APM
-Merged into single product node “AP” on the CAPS product tree, allowing all three models to be compared in the same grid
-Transitioned into new user experience
▶️ Video: CAPS Fan User Experience Improvements▶️
*Blower model USF
-No longer accepting orders for FC wheel (F1), F3 replacement still available
-VFD control package: ACS-320 replaced by ACH and ACS-180 where applicable
▶️ Watch the Inline Fans CAPS Training Video ▶️
*Quick Build (QB) lead time improvements on inline model SQ sizes 27-33 and select SQ/KSQ accessories/options
*Mixed flow inline model SQ
-Added High Wind rating option
-Performance baffle is available in sizes 7-12
-New fractional motor sizes added
*Roof supply model KSQ
-Added High Wind rating option
-Expanded fully assembled and shipped sizes
-SAF model is now obsolete, fully replaced by KSQ
*Roof supply and exhaust model RSQ
-Added High Wind rating option
-Added insulated hood option
*Roof supply model RSF and roof exhaust model LB will be obsoleted (replaced by RSQ)
*Replaced ABB VFDs with Danfoss VFDs on projects selected with a Vektor® system control package
*No changes
*Sound curb production moved to a new location
-Impacted models: ATI, ATIP, ATIR, ATS, ATR and ATE
-No Union Made label will be available
-Available in galvanized only (no coatings or aluminum)
*Updated location for stocked dampers from Accessories to Stock Products
📝 Read The Related Bulletin From: Michael Bulzomi- Sent 11/4/2024 📝
*AX Family (inline, upblast, supply, and reversible) transitioned into new user experience
▶️ Watch the CAPS Fan User Experience Improvements Video ▶️
*Models QEI and QEID multiple mark quantity bug fixed
Conditioning and Ventilating Products - Rep Partner CAPS 4.46 (Canada + INTL)
▶️ Watch The DOAS CAPS Training Video▶️
*New user interface for models RV, RVE, and RVC
*Heat-cool only third-party control configuration
📝 Read The Related Bulletin From: Mike Glodowski and Jennifer Butina 📝
▶️ Watch The ERV CAPS Training Video▶️
*New ERVi model
-Indoor, low-profile, modular construction
-Airflow ranges from 300 to 2,500 cfm
-1-inch injected foam cabinet
-EC, direct drive
▶️ Watch The KVS CAPS Training Video ▶️
*Expanded Amerex® fire suppression to allow for fusible link with Zone Defense systems
*Amerex® 2.50 gallon tank is now available for hood systems requiring 7 flow points or less
*Removed Amerex® 6.00 gallon tank based on low historic usage
*Fixed bug that prevented fans with the new user interface from linking to kitchen controllers
*Fixed field hook-up distributor selection bug that was resetting fire distributor selections
*Fixed UDS drawing bug that did not allow drawings to generate when filtered water was included
▶️ Watch The MUA CAPS Training Video ▶️
*Will accept orders for the new PDX with R454B refrigerant
📝 Read The Related Bulletin From: Dustin Woosley - Sent 10/21/2024 📝
*Updated drawings, wiring diagrams, and sequence of operations for the new PDX offering
📝 Read The Related Bulletin From: Mike Glodowski and Jennifer Butina 📝
Air Control Products - Rep Partner CAPS 4.46 (Canada + INTL)
▶️Watch The Dampers CAPS Training Video ▶️
*Enhanced user interface for heavy-duty round control (HCDR), round isolation (HBTR), rectangular backdraft (HB/HPR), and protection (HBS/HTOD) dampers. Enhancements include:
-Fast data entry
-Multi-line editing
-Global editing of grid entries
-Help text
-Conflict resolution
*Obsoleted user interface for air measuring, face & bypass, round backdraft, round fire smoke, and round control product families
*Obsoleted models HBS-331, 431; HTOD-331; HCD-324, 524
*Expanded selection for damper rep stock offering
*Factory-mounted FSKN BACnet® test module on FSD/SMD models
*Insulation depth on HCDR-350
*Replacement blade seal for heavy-duty bubble-tight (HBT/HBTR) dampers
*Best available lead time updated to 3-Day for ICD-44, 45; VCD-40, 42, 43, 43V; SMD-401EF, and EM Series dampers
*No longer available: Life Safety dampers with height equal to 8, but less than 9 inches, with an internal actuator that is not Belimo FSTF or Honeywell MSXX03 when an RRL is selected
*Updated rating for Siemens GJD series actuators used on control dampers
*Updated location for stocked dampers from Accessories to Stock Products
📝 Read The Related Bulletin - From: Michael Bulzomi - Sent 11/4/2024 📝
▶️ Watch The Louvers CAPS Training Video ▶️
*Equipment screen model EES-401 now has submittal drawings available for various configurations
*Added notification when the sections wide changes after a user manually changes the width or height
*Obsolesced thinline models ESU-153 and ESU-154
CAPS® 4.45
Canada and International
Air Movement Products - CAPS 4.45 (Canada + INTL - Reps)
- No changes
▶️ Watch the Ceiling Fans CAPS 4.45 Training Video ▶️
- SP-LP0511H(L) and SP-LP0810W(L) include a submittal callout for the specific integrated humidity sensor or two-speed capable option
- Obsoleted SP-A50-90-VG and SP-A90-130-VG models (covered by SP-AP0511W-1, SP-A200, SP-A390-VG)
- Obsoleted CRD (Ceiling Radiation Damper) with grille-mounted motion sensor and integrated dehumidistat for all SP-Bs and select SP-As
- Obsoleted 220, 230, and 240 volt motor options on the SP-B90, SP-B150, and SP-B200
- Removed aluminum and galvanized wheel options for the SP/CSP-A70, A90, A110, A125
- Removed stainless steel grille option for the SP-A700, A900, A1050, A1300, A1550
▶️ Watch the Centrifugal Fans CAPS 4.45 Training Video ▶️
- Plenum model APD - obsoleted BC and C1 wheels (covered by A1 wheel)
- Blower model USF - obsoleted F2 (forward curved) wheel
▶️ Watch the Inline Fans CAPS 4.45 Training Video ▶️
- Models SQ, BSQ, KSQ, and RSQ will have some user experience improvements
- SQ Mixed Flow Price Reductions
- Legacy SQ models with centrifugal wheels list price increases
- Quick Build Lead Time Improvements on SQ Mixed Flow
- New direct drive roof fan model RSQ
- 📝 Read The Related Bulletin 31-24 - From: Mike Bump - Sent 7/29/2024 📝
- Rooftop supply (filtered) and exhaust applications
- Sizes 7 thru 33
- Airflow up to 27,100 cfm and 3 in. wg.
- Vari-Green® up to 10 hp
- Spark B & C fan construction now available on model SQ Mixed Flow, KSQ, and RSQ sizes 12-33 with EXP motors
- Added performance baffles on model SQ Mixed Flow and KSQ sizes 7, 9, and 12 for higher pressures at lower flow rates
- SASO Certification (Saudi Standards, Metrology and Quality Organization) on SQ Mixed Flow, KSQ, and RSQ
- Obsoleted roof supply model SAF (covered by the KSQ and new RSQ)
- No changes
- No changes
▶️ Watch the Power Roof Ventilators and Roof Curbs (PRV) CAPS 4.45 Training Video ▶️
- Models G, GB, CUE, and CUBE will have some user experience improvements
- Models CUE and CUBE have new installation and service features
- 📝 Read the Related Bulletin 19-24 - From: Dave Mayer - Sent 5/20/2024 📝
- Removable power pack, toolless entry to motor compartment, lifting points, and dimensional adjustments
- Impacts the CUE and CUBE sizes 60 to 240
- Obsoleted IEC (International Electrotechnical Commission) motors
- Obsoleted EM-10 damper option
- Obsoleted the mounted curb cap adapters for G/GB sizes 300+
- Curb Seal default will be “Foam - Applied” on G/GB models when a curb is selected
- TEFC VG Motors will always show shaft grounding as “Yes”
- High Wind & Seismic option moved from the Construction tab to the Sizing tab
- Changed the name of the S.S. Fasteners option to be Fastener Material with answers of Standard/Stainless
- Changed the name of the S.S. Shaft option to Shaft Material with answers of Standard/Stainless
Conditioning and Ventilating Products - CAPS 4.45 (Canada + INTL - Reps)
▶️ Watch the DOAS CAPS 4.45 Training Video▶️
- New RVE-20 – includes polymer energy recovery wheel up to 2,000 cfm
- Enhanced roof curb drawings
- New R-454B refrigerant (replacing R-410A)
- Obsoleted Split DX Cooling
- Obsoleted RV-110, REV-180, RVC-145 (covered by RV-75 and RVE-150)
- Webinar: New in CAPS® 4.45 (DOAS & TAP)
▶️ Watch the KVS CAPS 4.45 Training Video ▶️
- Pollution Control Unit, model PCU updates
- Expanded fan offering to include Gen 2 USF fans
- Added fan selection flexibility based on brake horsepower, additional static head space, or cost
- Grease Trapper™ PCU Update
- Added ability to select specific arrangements of filters and modules on filtered PCUs
- Added BMS compatibility to filtered PCUs
- Added ability to increase housing size when lower brake horsepower and/or increase additional static is needed
- Crossover Hood - now configurable with a 6 in. front height
- Vari-Flow controls have been obsoleted (DCV selections should use PCB style system)
- Fixed cold water mist bug that was allowing cold water mist option on non-auto scrubber style hoods
- Fixed PCU IOMs bug that was not allowing PCU IOMs to generate
- Fixed supply collar positioning bug that was skewing supply collars in submittal drawings
- Amerex® fire system list pricing increased roughly 5%, resulted from supplier increase
▶️ Watch the MUA CAPS 4.45 Training Video ▶️
- DG-PDX units have been fully obsoleted and are no longer orderable
- FEI calculations have been updated to accommodate single phase for VG fan models
- Updated drawings for the GKD curbs on housings 35 and larger
- The hybrid centrifugal and larger mixed flow fan models have a 10% price increase
- Split DX cooling will no longer be selectable for new marks, previously selected units will remain orderable until September 23rd
- Packaged DX cooling selections with R410a will no longer be available, previously selected units will remain orderable until September 23rd
- New PDX design will be selectable after the September 23rd CAPS update, but not orderable until CAPS 4.46 on December 2nd
Air Control Products - CAPS 4.45 (Canada + INTL - Reps)
▶️ Watch the Dampers CAPS 4.45 Training Video ▶️
- Enhanced user interface for models HCD, HBT, and HBR (added fast data entry, multi-line editing, global editing)
- Stopped accepting orders from the old user interface for product families: ICD, MBD, VCD, and SMD-401EF
- New model HBT-321, heavy-duty rectangular damper for isolation and decontamination applications with AMCA 500-D
- Expanded Damper stock products offering to include: CRD-1, MBD-10, MBDR-50, VCDR-53, WD-200, WDR-53
- For models FSD/SMD, enhanced the grid to include blade indicator location and component location code
- Model OFSD, new 10-inch minimum height with RRL/OCI or TOR closure device
- Obsoleted models HCD-324 and 524
- Obsoleted stock products: BD-330-15x15, BD-330-17x17, WD-330-15x15, WD-330-17x17, WD-330-25x25, WD-330-30x30
- Obsoleted NEMA 3, 4, 4x enclosures for VCD-23V, 33V, 34V, 43V
- Obsoleted 10 gauge sleeve thickness for stainless steel FSD, SMD, VCD
- Added an override limits feature in the grid allowing selections beyond standard performance boundaries
- ▶️ Watch the Related Video: CAPS 4.45 Training - Louvers Override ▶️
- Added guidance (maximum volume recommendation) to the validation message when selecting by performance beyond standard performance boundaries
- Added project-specific submittal drawing capability to the new AFL-601 FEMA wind-driven rain louver
CAPS® 4.44
Canada
Air Movement Products - CAPS 4.44 (Canada - Reps)
▶️ Watch the Axial Fans CAPS 4.44 Training Video ▶️
- Lead Times
- AER with fabricated steel propeller lead times updated from extended to standard
- BAER sidewall propeller lead times updated from extended to standard
- Updated BAER pricing to be more competitive against competitors and SBE/SBS, SBCE/SBCS
- Axial hooded rooftop models
- Miami-Dade NOA was renewed (23-1122.03) so it has a new NOA number
- Florida Product Approval received with 2023 Florida Building Code (8th Edition)
- Obsoleted sidewall propeller models SE/S2 (all sizes), SBCE/SBCS/SBE3/SBS3 sizes 48 and smaller (recommend AER and BAER as the replacements) (no new selections)
- Increased performance on AER (sizes 20 – 30) and BAER with fabricated steel propeller (all sizes)
- Filtered wall housing added to BAER (sizes 24 – 48)
- Propeller guard added to BAER (sizes 24 – 36)
- Added ship loose Variable Frequency Drives for model AER
- Price adjustment on aluminum filters everywhere offered (SQ, KSQ, BSQ, SAF, RSF)
▶️ Watch the Ceiling Fans CAPS 4.44 Training Video ▶️
- No longer accepting orders for the following obsoleted products
- Whole House Ventilation for SP-B80 and SP-B110ES
- 220V to 240V motor selections for SP-A110 and SP-A390
- SP-A1410
- Started to obsolete (no new selections)
- Speed controller (internally and externally mounted), grille-mounted motion detector, grille-mounted dehumidistat, and metal wheels for sizes SP-A70 to SP-A125
- Mounted CRD option for SP-A110 and SP-A125
- 220V to 240V motor selections for SP-B90 and SP-B200, a message will pop up in this CAPS release (4.44) and will be fully obsoleted in CAPS 4.45
- Transformers moved to stock tree only
- New ship loose CRD (Ceiling Radiation Damper) for SP-LP0511H/HL and SP-LP0810W/WL (lighted and non-lighted)
▶️ Watch the Centrifugal Fans CAPS 4.44 Training Video ▶️
- Obsoleted direct-drive forward curved F2 wheel (sizes 6, 7, 9, 10) for model USF (no new selections)
▶️ Watch the Commercial Inline and Rooftop Fans CAPS 4.44 Training Video ▶️
- Standard lead-time improvements on SQ and KSQ mixed flow selections
- Expanded Quick Build on many SQ and KSQ mixed flow selections
- New 1/15 hp Vari-Green® motor on SQ and KSQ (reduced cost over larger horsepower)
- Addition of shipped loose VFD on SQ and KSQ mixed flow selections
- Price reduction on KSQ-12
- Price adjustment on aluminum filters everywhere offered (SQ, KSQ, BSQ, SAF, RSF)
- KSQ will now ship fully assembled (most sizes/selections)
- No changes
- No changes
▶️ Watch the Power Roof Ventilators and Roof Curbs (PRV) CAPS 4.44 Training Video ▶️
- PRV fan models CUE, CUBE, G, GB, AE, and AS are available to meet the requirements of California Title 20
- Low volume list price adjustments
- CUE-120-A, CUE-130-A, and CUE-140-A: 5-15% list price increase
- Hood Hasp option: $25 list increase
- Sound attenuating curbs (AT series): 12% list increase
▶️ Watch the Tubular Inline Fans CAPS 4.44 Training Video ▶️
- Obsoleted the TAUD and TDI (replaced by AX 200 Upblast series )
- Removed AX 200 series VG selections
Conditioning and Ventilating Products - CAPS 4.44 (Canada - Reps)
▶️ Watch the DOAS CAPS 4.44 Training Video ▶️
👨🏻🏫 Register for the DOAS Webinar in Bulletin 11-24 👨🏻🏫
- New A2L refrigerant (R-454B replaces R-410A) – EPA enforcement is 1/1/2025
- Obsolete models RV-110, RVE-180, and RVC-145 (no new selections)
- Split DX cooling phase-out
- 208 volt motor changes (impacts FLAs)
- No changes
▶️ Watch the KVS CAPS 4.44 Training Video ▶️
- Grease X-Tractor™ high-efficiency filters redesign for less static pressure
- 14 in. wide supply plenum now offers 10 in. and 12 in. wide rectangular collars and the 18 in. wide supply plenum now offers 14 in. and 16 in. wide rectangular collars
- Added appliance filter feature within hood marks to filter based on: most common, solid fuel, upper level, or all
- Vari-Flow legacy control is being obsoleted in CAPS v4.45 (no new selections in v4.44)
- UDS/UPS update prevents UPS from being selectable if UDS is selected without gas service
- Removed ability to select exhaust duct collar tight against exhaust top (min. 1 in. off back)
- Residential Range Hood, fixed bug that showed 500 cfm availability on front discharge models
- Greenheck Coordinated Field Fire install +10% list price increase (K11 to remain same) because of rising distributor labor rates
▶️ Watch the MUA CAPS 4.44 Training Video ▶️
👨🏻🏫 Register for the MUA Webinar in Bulletin 11-24 👨🏻🏫
- New factory-mounted and wired outlet damper option for DGX, MSX, and Greenheat models
- Diffusers are now available for the hybrid centrifugal fan types D1 and D3
- New touchscreen option for microprocessor control to replace the remote display option
- Insulated/non-insulated outlet damper options have been removed for all make-up air models
- CAPS 4.44 will be the last CAPS version that PDX will be available for the DG model
Air Control Products - CAPS 4.44 (Canada - Reps)
▶️ Watch the Dampers CAPS 4.44 Training Video ▶️
- New user interface for Access Door, Automatic Balancing, Backdraft, Ceiling Radiation, and Remote Balancing dampers includes:
- Fast data entry
- Multi-line editing
- Global editing
- Obsoleted models/options
- No longer accepting orders for:
- Obsoleted old user interface for models FSD, SMD, DFD, and/or FD product families
- Models FBH-23, 33, 43
- Models FBV-33, 43 – replaced by FBV-23
- Security Bars for DFD, FD, and VCD product families
- Stainless steel axle bearings and axle material for WD dampers
- No longer accepting orders for:
- Siemens GXVD series actuators default on select multiple section high FSD and SMD configurations
- List price increases for:
- Multiple actuator models
- Curtain Fire (DFD, FD) dampers
- VCD product family various low-volume options
▶️ Watch the Louvers CAPS 4.44 Training Video ▶️
- Performance-based selection by volume added to the Fast Data Entry selection tool for both intake and exhaust applications
- Configuration tab enhancements:
- Allow changes right in the line for the volume-based performance selection
- Show volume, velocity, and pressure drop performance info when volume is provided
- An approximate 70% price increase on 1” and 2” permanent washable filters when selected as an option with the louvers
- Some actuator model price increases to be aligned with any damper actuator pricing increase
- Select sizes of model ESD-635DE (Miami-Dade) are no longer available on QD Stock
- NEW! AFL-601 Wind-Driven Rain FEMA Louver Model (6-inch deep, ICC 500 impact qualification)
International
Air Movement Products - CAPS 4.44 (INTL- Reps)
▶️ Watch the Axial Fans CAPS 4.44 Training Video ▶️
- Lead Times
- AER with fabricated steel propeller lead times updated from extended to standard
- BAER sidewall propeller lead times updated from extended to standard
- Updated BAER pricing to be more competitive against competitors and SBE/SBS, SBCE/SBCS
- Axial hooded rooftop models
- Miami-Dade NOA was renewed (23-1122.03) so it has a new NOA number
- Florida Product Approval received with 2023 Florida Building Code (8th Edition)
- Obsoleted sidewall propeller models SE/S2 (all sizes), SBCE/SBCS/SBE3/SBS3 sizes 48 and smaller (recommend AER and BAER as the replacements) (no new selections)
- Increased performance on AER (sizes 20 – 30) and BAER with fabricated steel propeller (all sizes)
- Filtered wall housing added to BAER (sizes 24 – 48)
- Propeller guard added to BAER (sizes 24 – 36)
- Added ship loose Variable Frequency Drives for model AER
- Price adjustment on aluminum filters everywhere offered (SQ, KSQ, BSQ, SAF, RSF)
▶️ Watch the Ceiling Fans CAPS 4.44 Training Video ▶️
- No longer accepting orders for the following obsoleted products
- Whole House Ventilation for SP-B80 and SP-B110ES
- 220V to 240V motor selections for SP-A110 and SP-A390
- SP-A1410
- Started to obsolete (no new selections)
- Speed controller (internally and externally mounted), grille-mounted motion detector, grille-mounted dehumidistat, and metal wheels for sizes SP-A70 to SP-A125
- Mounted CRD option for SP-A110 and SP-A125
- 220V to 240V motor selections for SP-B90 and SP-B200, a message will pop up in this CAPS release (4.44) and will be fully obsoleted in CAPS 4.45
- Transformers moved to stock tree only
- New ship loose CRD (Ceiling Radiation Damper) for SP-LP0511H/HL and SP-LP0810W/WL (lighted and non-lighted)
▶️ Watch the Centrifugal Fans CAPS 4.44 Training Video ▶️
- Obsoleted direct-drive forward curved F2 wheel (sizes 6, 7, 9, 10) for model USF (no new selections)
▶️ Watch the Commercial Inline and Rooftop Fans CAPS 4.44 Training Video ▶️
- Standard lead-time improvements on SQ and KSQ mixed flow selections
- Expanded Quick Build on many SQ and KSQ mixed flow selections
- New 1/15 hp Vari-Green® motor on SQ and KSQ (reduced cost over larger horsepower)
- Addition of shipped loose VFD on SQ and KSQ mixed flow selections
- Price reduction on KSQ-12
- Price adjustment on aluminum filters everywhere offered (SQ, KSQ, BSQ, SAF, RSF)
- KSQ will now ship fully assembled (most sizes/selections)
- No changes
- No changes
▶️ Watch the Power Roof Ventilators and Roof Curbs (PRV) CAPS 4.44 Training Video ▶️
- PRV fan models CUE, CUBE, G, GB, AE, and AS are available to meet the requirements of California Title 20
- Low volume list price adjustments
- CUE-120-A, CUE-130-A, and CUE-140-A: 5-15% list price increase
- Hood Hasp option: $25 list increase
- Sound attenuating curbs (AT series): 12% list increase
▶️ Watch the Tubular Inline Fans CAPS 4.44 Training Video ▶️
- Obsoleted the TAUD and TDI (replaced by AX 200 Upblast series )
- Removed AX 200 series VG selections
Conditioning and Ventilation Products - CAPS 4.44 (INTL- Reps)
▶️ Watch the DOAS CAPS 4.44 Training Video ▶️
👨🏻🏫 Register for the DOAS Webinar in Bulletin 11-23 👨🏻🏫
- New A2L refrigerant (R-454B replaces R-410A) – EPA enforcement is 1/1/2025
- Obsolete models RV-110, RVE-180, and RVC-145 (no new selections)
- Split DX cooling phase-out
- 208 volt motor changes (impacts FLAs)
- No changes
▶️ Watch the KVS CAPS 4.44 Training Video ▶️
- Grease X-Tractor™ high-efficiency filters redesign for less static pressure
- 14 in. wide supply plenum now offers 10 in. and 12 in. wide rectangular collars and the 18 in. wide supply plenum now offers 14 in. and 16 in. wide rectangular collars
- Added appliance filter feature within hood marks to filter based on: most common, solid fuel, upper level, or all
- Vari-Flow legacy control is being obsoleted in CAPS v4.45 (no new selections in v4.44)
- UDS/UPS update prevents UPS from being selectable if UDS is selected without gas service
- Removed ability to select exhaust duct collar tight against exhaust top (min. 1 in. off back)
- Residential Range Hood, fixed bug that showed 500 cfm availability on front discharge models
- Greenheck Coordinated Field Fire install +10% list price increase (K11 to remain same) because of rising distributor labor rates
▶️ Watch the MUA CAPS 4.44 Training Video ▶️
👨🏻🏫 Register for the MUA Webinar in Bulletin 11-24 👨🏻🏫
- New factory-mounted and wired outlet damper option for DGX, MSX, and Greenheat models
- Diffusers are now available for the hybrid centrifugal fan types D1 and D3
- New touchscreen option for microprocessor control to replace the remote display option
- Insulated/non-insulated outlet damper options have been removed for all make-up air models
- CAPS 4.44 will be the last CAPS version that PDX will be available for the DG model
Air Control Products - CAPS 4.44 (INTL- Reps)
▶️ Watch the Dampers CAPS 4.44 Training Video ▶️
- New user interface for Access Door, Automatic Balancing, Backdraft, Ceiling Radiation, and Remote Balancing dampers includes:
- Fast data entry
- Multi-line editing
- Global editing
- Obsoleted models/options
- No longer accepting orders for:
- Obsoleted old user interface for models FSD, SMD, DFD, and/or FD product families
- Models FBH-23, 33, 43
- Models FBV-33, 43 – replaced by FBV-23
- Security Bars for DFD, FD, and VCD product families
- Stainless steel axle bearings and axle material for WD dampers
- No longer accepting orders for:
- Siemens GXVD series actuators default on select multiple section high FSD and SMD configurations
- List price increases for:
- Multiple actuator models
- Curtain Fire (DFD, FD) dampers
- VCD product family various low-volume options
▶️ Watch the Louvers CAPS 4.44 Training Video ▶️
- Performance-based selection by volume added to the Fast Data Entry selection tool for both intake and exhaust applications
- Configuration tab enhancements:
- Allow changes right in the line for the volume-based performance selection
- Show volume, velocity, and pressure drop performance info when volume is provided
- An approximate 70% price increase on 1” and 2” permanent washable filters when selected as an option with the louvers
- Some actuator model price increases to be aligned with any damper actuator pricing increase
- Select sizes of model ESD-635DE (Miami-Dade) are no longer available on QD Stock
- NEW! AFL-601 Wind-Driven Rain FEMA Louver Model (6-inch deep, ICC 500 impact qualification)