Greenheck Introduces ABD-Z2 Automatic Balancing Damper For Zone Register Terminals
April, 2022
The ABD-Z2 is the latest addition to Greenheck’s line of automatic balancing dampers that provide precise airflow regulation for energy efficient indoor air quality. The ABD-Z2 is an integrated automatic balancing damper (ABD) with an adjustable set point controlled by an electric actuator (24V or 120V). The unit can toggle between two
Greenheck Automatic Balancing Damper - Model ABD-Z2pressure independent CFM setpoints; the low-flow setpoint maintains a constant minimum ventilation rate, while the high-flow setpoint provides boosted on-demand ventilation. The ABD-Z2 helps achieve the requirements of ASHRAE 62.2 for acceptable indoor air quality and is ideal for use in apartments and condominiums, education buildings and dormitories, hospitals and clinics, hotels and motels, and nursing homes and assisted living facilities.

Greenheck, the worldwide leader in manufacturing and distributing air movement, control and conditioning equipment, offers the most UL certified dampers and the largest selection of AMCA licensed dampers in the industry.

For more information, visit www.greenheck.com/products/air-control/dampers/abd-z2.

About Greenheck

Greenheck is a global leader in engineering and manufacturing air movement, control and conditioning equipment. For 75 years, we have been committed to promoting the highest levels of indoor air quality by offering the widest range of ventilation products for commercial and institutional buildings. Through superior customer service, we continue our legacy of innovation as experts in air movement by connecting our mechanical representative partners and customers with the newest products. With our CAPS® product selection tool and HVAC University product education series, Greenheck offers technology and product knowledge to ensure that when you work with us, you are working with the easiest company to do business with.

To learn more, visit www.greenheck.com or contact Greenheck, P.O. Box 410, Schofield, WI 54476-0410, (715) 359-6171, FAX (715) 355-2399.