Greenheck Introduces Three-Phase Vari-Green® Motors
October, 2020
Greenheck has added three-phase motors to its line of energy efficient Vari-Green® electronically commutated (EC) motors. The new three-phase motors accept 208-230V and 460V power supply and are available in sizes ranging from 1 to 10 hp. Typical turndown is
factory-set at 75% and speed can be controlled via an onboard dial or a 0-10 VDC control signal. Low maintenance Vari-Green motors run quieter and cooler and offer higher efficiencies compared to standard motors; the three-phase Vari-Green motor operates at IE5 efficiency levels. The three-phase motor is compatible with all Vari-Green controls and other controls such as a building automation system and has an auxiliary contact for motor status or damper actuation. The three-phase Vari-Green motor can be ordered with select sizes of Greenheck models SQ inline fans, AER axial fans and models G and CUE power roof ventilators.
Greenheck is the worldwide leader in manufacturing and distributing air movement, conditioning and control equipment.
For more information about Greenheck products, visit www.greenheck.com or contact Greenheck, P.O. Box 410, Schofield, WI 54476-0410, (715) 359-6171, FAX (715) 355-2399.

Greenheck is the worldwide leader in manufacturing and distributing air movement, conditioning and control equipment.
For more information about Greenheck products, visit www.greenheck.com or contact Greenheck, P.O. Box 410, Schofield, WI 54476-0410, (715) 359-6171, FAX (715) 355-2399.