Greenheck Model DS Named to Retrofit Magazine’s Top 50 Product List
March 2020
Retrofit magazine recently recognized Greenheck model DS high volume low speed (HVLS) fan as one of the publication’s Top 50 Products of 2019. The recognition is the result of the publication asking its readers to identify the most interesting products from their magazine over the past year. 
The HVLS fan offers eight sizes ranging from 8 to 24 feet in diameter and has an optimized design for maximum efficiency and coverage. Model DS is currently the only HVLS fan licensed to bear the AMCA Seal for Circulating Fan Performance. The fan provides up to 243,000 cfm and uses quiet direct drive technology, making it up to 10 dBA quieter and 20% more efficient than comparable HVLS fans.
The top 50 list featuring model DS, appeared in the January/February 2020 issue. To read the article, visit Retrofit magazine.

The HVLS fan offers eight sizes ranging from 8 to 24 feet in diameter and has an optimized design for maximum efficiency and coverage. Model DS is currently the only HVLS fan licensed to bear the AMCA Seal for Circulating Fan Performance. The fan provides up to 243,000 cfm and uses quiet direct drive technology, making it up to 10 dBA quieter and 20% more efficient than comparable HVLS fans.
The top 50 list featuring model DS, appeared in the January/February 2020 issue. To read the article, visit Retrofit magazine.