Roof Mounted Fans-FAQQA7
What is the maximum roof pitch that a fan can be mounted to without correcting the curb for the pitch?
Link text :
Select a Card/Question Answer :
QuestionAnswer
Display order :
7
As a rule, the recommended maximum roof pitch is 2:12 or 10 degrees from horizontal. Steeper pitches will increase the possibility of moisture infiltration into the building as a result of water splashing off the roof and entering the fan. For roof pitches greater than 2:12, it is recommended to have a pitched curb, which will allow the fan to sit level and not at an angle.
faqcategories :
- Roof Mounted Fans FAQs
Related pages :
from