Greenheck Model ECV-40 Named to Retrofit Magazine's Top 25 Products List
January, 2021
Retrofit magazine recently recognized Greenheck model ECV-40 as one of the publication’s Top 25 Products of 2020. The eighth annual Top 25 Products, which appears in Retrofit’s January/February 2021 issue, celebrates the products that received the most reader inquiries from the magazine’s November/December 2019 through September/October 2020TOP-25_Logo_2020 issues.

The ECV-40’s design features a dual-fan arrangement consisting of direct drive mixed-flow plenum fans with variable frequency drives (VFDs) replacing the forward-curved fan typically found in energy core ventilators. The mixed flow fan, a hybrid between an axial propeller and centrifugal fan, reduces brake horsepower requirements by up to 50%. The VFDs facilitate ease of balancing at start-up. Sound power levels are reduced, and no belts make maintenance easy. 

Retrofit is the only print and online publication exclusively dedicated to covering the renovation of existing commercial, institutional and industrial buildings. Published bimonthly, the magazine is nationally circulated to approximately 45,000 architects, contractors, facility managers, building owners and government officials.

To read the article, visit Retrofit magazine.