Energy Recovery Ventilators Frequently Asked Questions
Q: What is the energy recovery wheel made of?
Greenheck energy recovery products use a "total energy recovery" or
"enthalpy" wheel. The energy transfer media in the wheel is constructed
of lightweight polymer with permanently imbedded silica gel desiccant.
The polymer media transfers the sensible heat, while the silica gel
desiccant transfers the moisture or latent energy.
Q: Does the energy recovery wheel act like a filter?
No. These products are designed to induce laminar or smooth airflow,
which allows small particles to pass through the wheel. Pre-filters are
available to prevent dust and other outdoor pollutants from entering the
building. Larger particles, which may impinge on the wheel surface, are
blown off as the wheel rotates into the other, counter-flowing air
stream.
Q: What is the expected life of the energy recovery wheel?
he energy recovery wheels used in Greenheck products have been operating
in commercial and institutional buildings for over 10 years. In that
time, performance of these wheels has been excellent and only occasional
freight and installation damage has been cause for replacements. In
addition to a long, reliable history of performance, Greenheck warrants
the energy recovery wheel for five years.
Q: How much cross leakage is expected through the energy recovery wheel?
Cross leakage through the energy recovery wheels ranges from 2% to 5%
between the supply and exhaust air streams. This amount of cross leakage
is minimal and in comfort ventilation applications is perfectly
acceptable. These leakage rates are also acceptable for Class 3 Air
(toilet room exhaust). According to ASHRAE Standard 62-89R committee, up
to 10% cross leakage of Class 3 Air is acceptable for the purposes of
energy recovery.
Q: How does the total energy wheel compare to flat plate exchangers in
energy transfer efficiencies?
Metal flat plate exchangers transfer sensible heat (temperature) only
and do not transfer moisture (latent), which reduces the total
effectiveness of the energy transfer. A 75% efficient plate typically
only has a total effectiveness of 30%. Even plates, such as the
Mitsubishi Lossany core, transfer limited latent energy. Latent
effectiveness for Lossany typically is in the 40% to 50% range.
Greenheck energy recovery products transfer moisture, as well as
sensible heat. Our wheel is about 70%-80% efficient in both latent and
sensible. (Lower velocity will tend to have higher efficiency.) This
dramatically increases the total effectiveness of the energy exchange
and significantly shortens the pay back period of the unit. The April
1997 Update had an insert article titled "Plates vs. Wheels", which
addresses this question in much greater detail. The Greenheck web-site
contains several technical articles including "Plates vs. Wheels".
Q: How is the energy recovery wheel cleaned? What can be used to clean it?
Cleaning can start after the wheel media is removed from the cassette
housing. The energy wheel media can be cleaned in any of the following
ways:vacuumingsoaking the wheel media in cleaner or detergent/water
solutionspraying the wheel media with cleaner and brushing through
pressure washing (on a low setting). Details on cleaning are on page 17
of the ERV 1998 IOM. Cleaning fluid temperatures should be kept below
140°F, otherwise damage to the media could occur.
Q: Where can energy recovery be used?
Energy recovery can be applied in any commercial or institutional
comfort ventilation application. Some examples of applications:
Educational facilities: Schools, Dormitories, and Offices.Commercial
facilities: Office buildings, hotels/motels, beauty/nail salons, retail
stores, and restaurants.Institutional facilities: Nursing homes or
assisted living buildings.Public buildings: Fire and police stations,
jails and prisons, military facilities. The pay back period of an ERV is
quickest in an application meeting the following criteria:Air
conditioned buildings requiring outdoor ventilation air. Climate has a
0.4% design wet bulb greater than or equal to 75°F or a design dew point
greater than 66°F. The Southeastern, Midwestern and Eastern United
States have excellent climates for energy recovery. Energy recovery pay
back is lengthened in the Western part of the US due to climatic
conditions. However, there are still many applications and climates
where energy recovery provides significant benefits.Buildings with long
hours of operation, like nursing homes, fire stations or retail stores.
Q: Is the ERV performance data certified?
Currently, only the air performance on Greenheck ERVs is certified
through AMCA. The American Refrigeration Institute (ARI) and the
American Society of Heating, Refrigeration Engineers (ASHRAE) are
currently defining energy transfer ratings and test methods,
respectively. Both will be completed within the next year. Greenheck has
taken a proactive role on the ratings committee helping to define
proposed test methods and rating systems for energy transfer in energy
recovery technology.
Q: Can we incorporate supplemental heating and/or cooling devices into the
ERV?
Yes, using our Model ERT. This model allows downstream heating and
cooling of the preconditioned air from the energy recovery wheel. The
available cooling options are direct expansion (DX) coils or chilled
water coils. The heating options are electric heat or hot water coils.
Q: Is it difficult to change an ERV wired for 460/60/3 to 208/60/3?
When you have an ERV wired for the wrong voltage, it can be corrected.
However, voltage change outs on ERVs are time consuming and expensive.
Several components must be changed out including: Fan motors, if the
motors are not multi-voltage. Fan drives, if the motor frame size
changes. Motor starters, contactors and overloads will need to be changed
out in most cases. Disconnect size may change. Wiring will need to be
rerun to handle higher amp draws at the lower voltage. Please double
check voltage requirements before releasing orders.
Q: What is desiccant dehumidification?
Desiccant dehumidification includes a heating device (regenerator) in
the exhaust air stream to raise air temperature to 140 degrees F or
greater. The hot air causes most of the moisture to be released from the
wheel. The result is a capability to dry outdoor air to very low
humidity levels (as low as 10 grains of moisture/lb of air). Desiccant
dehumidification equipment is expensive and consumes a lot of energy
with the regeneration process. It is really designed for processes
requiring very dry air. Comfort ventilation applications are really a
misapplication of this product.
|