Greenheck Expands Miami-Dade Certified Louvers
December, 2005

Greenheck is expanding its Miami-Dade County Hurricane louver line by offering a new Miami-Dade approved louver model. The ESS-501D is a five-inch drainable blade model in a sightproof configuration. Greenheck is one of the first louver manufacturers to offer a Miami-Dade approved sightproof model, which can be used in coastal areas where louvers must be hurricane-resistant as well as aesthetically pleasing.
Greenheck’s Miami-Dade louver product line now includes four models—the most in the industry. Greenheck, an industry leader in the development, design, and application of severe duty products, manufactures the most AMCA-licensed louvers in the industry and offers unlimited custom louver engineering capabilities.
To obtain more information about this Greenheck announcement you may:
- Request information via e-mail
- Contact your local Greenheck Representative
- Phone us at (715) 359-6171 or fax us at (715) 355-2399
- Write us at Greenheck, P.O. Box 410, Schofield, WI 54476-0410