New high-capacity rooftop energy recovery ventilator; plus Model EQB wins an award
Home | Green | About Greenheck | Parts | Find My Rep | Careers | Contact Us

Greenheck has expanded its packaged rooftop ventilation line with the addition of Model RV(E)-120, a pre-engineered system featuring increased performance capabilities for larger dedicated outdoor air systems, multi-zone VAV systems, and single-zone VAV systems.

Model RV(E)-120 has two-inch foam insulated, thermally broken panel design construction. Low sound condenser fans for quieter operation are an average of 5-10dB less than standard condensing fans. Dual supply and exhaust fans deliver improved performance as well as reduced unit electrical loads. Four independent cooling circuits allow for excellent cooling turn down and control. On indirect gas-fired furnaces, 10:1 modulating turndown is available for increased operating performance. With performance capacities up to 12,000 cfm, up to 45 tons of cooling and up to 800 Mbh heating, Model RV(E)-120 meets the demands of today’s heating, cooling, dehumidification, and ventilation requirements.

Retro Fitting Fans in Existing Buildings?

Watch Video

The video demonstrates how to take apart and reassemble a centrifugal single width (CSW) fan with a quad split housing for retro fit applications requiring fans to be disassembled for installation.

We show you the tools needed as well as step-by-step instructions.

Like Us Now

Application Articles

Motor Application Guide
for Ventilation Products

The evaluation of a fan's motor is a time consuming part of the design of air handling equipment. This article will aid in the selection of the correct motor type from an electrical and mechanical standpoint for a given application and fan type.

Educational Info

Fan Accessories
Earn PDH

Most fans have common accessories that can be added to the basic model if required. This module will cover the following fan accessories: Electrical controls, Guards, Dampers and Vibration isolation.


Did You Know?

Model EQB wins a Dealer Design Award

The Model EQB received a Bronze award in the Ventilation Product category of the Dealer Design Awards. The award was judged by a panel of independent HVACR contractors selected by the editorial staff of The News.


Facebook Linkedin YouTube
Volume 7, Issue 4, August 26, 2015
©2015 Greenheck Fan Corporation
Greenheck • PO Box 410 • Schofield, WI 54476 • 715.359.6171