| Home | Green/LEED | About Greenheck | Find My Rep | Careers | Contact Us |
![]() |
| Products | Industries & Applications | Quick Delivery | Library | Software | Drawings | What's New |
Greenheck CAPS 4.8 Release – Important Information |
|
Dear CAPS Application User, Greenheck CAPS 4.8 Release Requires Microsoft .NET 4.0 Framework Upgrade CAPS 4.8 will be updated from version 4.6 in late January, 2012 and will include many new products and features. However, to update to CAPS 4.8 you must install Microsoft .NET Framework 4 on each computer workstation if it is not already present. Testing has shown it will take approximately 10 minutes to install Microsoft .NET Framework 4. To save approximately 10 minutes of download time in January, we encourage you to download the Microsoft .NET Framework today. To download, click on the link below. To download Microsoft .Net Framework 4, click here. http://www.microsoft.com/downloads/en/details.aspx?FamilyID=0a391abd-25c1-4fc0-919f-b21f31ab88b7 Following are the technical specs for Microsoft .NET Framework 4.
Note: The CAPS update process will include the download of .NET Framework 4 if you do not have it installed on your computer. However, the installation of the .Net Framework 4 will add an additional 10 minutes to the overall download time. If you have any questions, please feel free to contact Jody Meyer, Systems Specialist at jody.meyer@greenheck.com. |
|
Volume 3, Issue 9, December 7, 2011 ©2011 Greenheck Fan Corporation Greenheck • PO Box 410 • Schofield, WI 54476 • 715.359.6171 |