UL Certified horizontal damper solutions; plus Vektor-C Series
Home | Sustainability | About Greenheck | Parts | Find My Rep | Careers | Contact Us| National Accounts

Greenheck has revolutionized the ability to protect openings in horizontal partitions with the introduction of the industry's first line of fire and combination fire/smoke dampers approved for installation in horizontal, non-concrete fire rated barriers.

Prior to this newest technology, there was not a product in the market that satisfied code requirements when installed in any type of horizontal-rated barrier other than one constructed of load bearing concrete. This limitation brought about several challenges as the advancement of building design and construction practices evolved. This is especially true with regard to the protection of the top and bottom terminations of commonly used fire-rated shaft assemblies.

As old practices become obsolete, so do the conventions that drive them. Modern structures demand greater flexibility from building products and broader adaptability to installation concerns. Greenheck's new UL Certified horizontal damper solutions provides designers and installers with unparalleled versatility for complying with code requirements, without compromising creativity and efficiency.

VektorŪ-C - What You've Been Missing

Learn More

The next time you need a lab or fume exhaust fan, consider the VektorŪ-C series of pre-engineered systems.

Along with the traditional CD (dilution), the new CH (high plume) and CS (variable geometry nozzle) models provide more opportunity to beat the competition in performance and price.

Like Us Now

Application Articles

Actuators for Industrial
HVAC/Process Dampers

Selection of the actuator for a specific damper requires you to consider a number of factors. This article will examine the actuator selection process.

Educational Info

Fan Bearings
Earn PDH

Review important aspects of bearings, specifically related to air handling operation. This module will cover the following topics: Types, Housing and mounting systems, locking types, air handling quality design, basic rating life and maintenance.


Did You Know?

Manufacturing Day 2015

Manufacturing Day℠ is a celebration of modern manufacturing meant to inspire the next generation of manufacturers.


Facebook Linkedin YouTube
Volume 7, Issue 5, October 14, 2015
©2015 Greenheck Fan Corporation
Greenheck • PO Box 410 • Schofield, WI 54476 • 715.359.6171