Allow Popups
If you do not have pop-ups enabled on your browser, the site may not display as designed. To enable your browser for pop-ups follow the steps that apply to the browser you are using.
Note: Some security software and toolbars may also block pop-ups.
PC Users
Internet Explorer 6.0 on operating system Windows XP Service Pack 2
- From Tools point to Pop-up Blocker, and then click on Pop-up Blocker Settings
- Type www.qantas.com.au in the box 'Address of Web site to allow' and click Add
- Set the Filter Level to Medium: Block most automatic pop-ups
- Click Close
Firefox 1.0.x
- From Tools select Options
- Select the Web Features icon
- Ensure Block Pop-up Windows is not checked
- Click OK
Alternatively:
- From Tools select Options
- Select the Web Features icon
- Click Allowed Sites
- Type www.qantas.com.au into the field
- Click Allow
- Click OK
Mozilla 1.7.x
- From Edit select Preferences
- From the left hand side menu, click on + to open Privacy & Security
- Under Pop-up Windows, tick the check box for 'Block unrequested pop up windows'
- Then select Allowed Sites
- Type www.qantas.com.au in the box 'Allow pop-ups from the following web sites' and click Add
- Click OK
- Click OK
Opera 8.x
- From Tools select Preferences
- Under the General tab ensure 'Block unwanted pop-ups' is activated in the Pop-ups drop down box
- Click OK
Note: When using 'Block Unwanted Pop-ups', your result on our Viewing Tips page will still be FAILED, yet pop-ups will work. A PASS will only be noted if you select 'Open pop-ups in background' or 'Open all pop-ups'.
Netscape 7.x
- From Edit select Preferences
- From the left hand side menu, click on + to open Privacy & Security
- Under Pop-up Windows, ensure the 'Suppress pop-ups' radio button is selected
- Then select Exceptions
- Type www.qantas.com.au into the field and click Add
- Click OK
Mac Users
Opera 8.x
- From Opera select Preferences
- Under the General tab ensure 'Block unwanted pop-ups'^ is activated in the Pop-ups drop down box
- Click OK
Note: When using 'Block Unwanted Pop-ups', your result on our Viewing Tips page will still be FAILED, yet pop-ups will work. A PASS will only be noted if you select 'Open pop-ups in background' or 'Open all pop-ups'.
Safari 1.3.x and Safari 2.x
- From the Safari menu, ensure 'Block pop-up windows' is unchecked
Mozilla 1.7.x
- From Mozilla select Preferences
- From the left hand side menu click on + to open Privacy & Security
- Under Pop-up Windows, tick the check box for 'Block unrequested pop-up windows'
- Then select Allowed Sites
- Type www.qantas.com.au in the box 'Allow pop-ups from the following web sites' and click Add
- Click OK
- Click OK
Netscape 7.x
- From Netscape select Preferences
- From the left hand side menu, click on + to open Privacy & Security
- Under Pop-up Windows, tick the check box for 'Block unrequested pop-up windows'
- Then select Allowed Sites
- Type www.qantas.com.au into the field and click Add
- Click OK