PHILOSOPHY

Putting ourselves to the test.

“Design. Test. Certify.” This statement captures our commitment to the ventilation industry and to the development of quality air moving and control equipment.

Design – Innovation Leading the Industry Forward

Greenheck engineers lead the industry in innovative product solutions. The input for these solutions comes from hundreds of manufacturer representatives around the world. They listen to their customers and relay that information. Our advanced computer modeling and testing capabilities aid the collaboration. The result is a high-performance product manufactured using precise methods to provide an easy, low-cost installation.

This process from customer to the rep and finally our engineers has one goal: delivering value that exceeds our customers’ expectations. Just look at our compact fans with the lowest sound levels and highest efficiencies. You will see innovation everywhere.
Innovation-Center-Testing
Fan Test

Performance Assurance

Product testing and qualification play a major role in Greenheck’s heritage and success. We conduct rigorous testing in world-class laboratories ensuring that all designs and purchased parts meet quality standards that Greenheck customers have come to expect.

Real-life, in-house testing procedures measure aerodynamic performance, sound levels, structural integrity, mechanical operation, environmental impact, temperatures, vibration levels and more. Fans are put through air and sound testing; louvers are tested for water penetration and pressure drop. Dampers are scrutinized in fire life safety testing.

In addition to performance testing, Greenheck products go through rigorous structural testing. Fans, dampers and louvers are put through life tests and cycle tests. Components such as belts, pulleys, bearings and motors are also life tested. Motors are stressed in overload and over/under voltage tests, while bearings must pass extensive L10 life verification tests. Here is just a sample of the many product development tests we use at Greenheck:

  • Air performance testing
  • Sound performance testing
  • Psychrometric testing
  • Product development prototyping & training
  • Structural testing
  • Overspeed testing
  • Endurance testing
  • UL/ETL temperature testing
  • UL restaurant exhaust (grease) testing
  • UL power ventilators for smoke control (high temperature) testing
  • Hurricane testing
  • Finite element analysis (FEA)
  • Computational fluid dynamics (CFD)
  • Modal testing
  • Fatigue testing
  • Motor testing
  • Actuator testing
Wheel-Test-Failure
Wheel Failure Test

Certify – Making the Grade

Greenheck performs extensive testing on its products. As a result, we offer more products with certifications from AMCA, UL, CE, NOM, ETL, CSA and ULc than any other manufacturer in the industry. Four in-house, third-party registered air chambers and a registered sound-testing facility are maintained to the highest standards of the accrediting organizations. These third-party certifications ensure Greenheck products fulfill customers’ expectations.
Prop-Strength-Test
Fatigue Blade Cycle Test

International Testing Standards

Testing standards are the same as our U.S. products.