Madison,
Wisconsin Fire Station #11
Madison, WI
Printable Case Study
Madison.pdf

Architectural
&
Engineering Firm:
Hein Engineering Group
Madison, WI |
Architectural
Firms::
Plunkett Raysich Architects
Madison, WI |
General
Contractor:
Miron Construction
Madison, WI |
|
The
Challenge
- Help
save energy by reducing cooling costs where no natural
shade exists.
- Create
an appealing outdoor gathering area for the resident
firefighters and public visitors.
- Design
sunshades that contribute to the overall aesthetic goals
of the architect and that are able to tolerate heavy
snow loads in the winter.
A newly constructed fire station in an attractive, but
undeveloped new urban community in Madison, Wisconsin
was designed to make a statement in the neighborhood and
set the tone for future commercial, retail and residential
development. Faced with a treeless sloping prairie and
overlooking a wetland and prairie grasses, the architect
and City of Madison officials wanted this first public
building to communicate a restrained civic presence by
conveying importance – without being pretentious.
The greatest challenge of this project was to site the
building so that the functional requirements of the fire
station were in balance with the importance of defining
the street edge in this pedestrianoriented neighborhood.
Long, flat drive-in and drive-out lanes necessitated that
the building was pulled back from each street corner,
but city officials and the architect wanted to make sure
area residents walking past the building were well aware
that emergency vehicles might appear at any second. In
addition, because the station was a publicly funded building
with a community room for neighborhood meetings, officials
wanted Fire Station #11 to reflect a warm, friendly and
inviting feeling.
Greenheck's Solution
- Custom
architectural sunshades.
- Two
custom freestanding architectural sun-controlled areas.
- Custom
form Bullnose fascia.
To
add depth to the building and to help reduce cooling costs,
Greenheck designed and manufactured a unique sunshade
control area that consists of free-standing clear, anodized
sunshades at the front entrance to the fire station. Freestanding
supports were strategically located to complement vertical
sightlines of windows and other building lines. To hide
fastening hardware, Greenheck designed a custom 12-inch
bullnose fascia that wrapped around the perimeter of each
sunshade. Maximum shading was achieved with blades tilted
at a standard 45 degree angle.
Architectural sunshades also were installed 25 feet above
the ground level over an upper row of windows above the
fire engine garage doors to allow firefighters to keep
windows open for maximum fresh air ventilation during
peak hours of sunshine. To complement the building’s
clean lines and aesthetic appeal, these sunshades projected
six feet from the building. The six foot extension required
a special aluminum support tied to the foundation to tolerate
heavy snow loads in the winter. Finally, a 25 foot x 35
foot freestanding sun-controlled area with clear anodized
sunshades was created to maximize shade over a patio and
barbecue area during the hot summer months in Madison.
The Results
- The
Madison Fire Station #11 is an attractive new addition
to the city’s east side neighborhood.
Pedestrians strolling past the sleek new station admire
the friendly, sunshaded areas that project outward from
the front of the building, and often stop to visit with
firefighters under the sunshaded outdoor patio. Double
rows of trees have been planted alongside the building
and when mature will further cool the site and make the
building even more inviting.