Kansas
Life Sciences Innovation Center
Kansas City, KS
Printable Case Study
kansas_life_center .pdf

Owner:
University of Kansas Medical Center
Kansas City, KS |
Engineering
Firms:
Cannon Design
St. Louis, MO |
Architectural
Firm :
GLPM Architects, Inc.
Lawrence, KS |
Contractors:
Turner Construction Company, General
Contractor,
Kansas City, MO
Midwest Mechanical Contractors, Inc.
Kansas City, MO
Barnes and Dodge, Inc., Installing
Contractor,
Kansas City, KS
|
Greenheck
Representative:
Jorban-Riscoe Associates
Lenexa, KS |
|
The
Challenge
- Efficiently
remove and dilute large volumes of laboratory exhaust
air high above the surrounding campus and neighborhoods.
- Construct
a reliable lab exhaust system with low maintenance.
- Minimize
distractions from the building's impressive exterior
aesthetics.
Construction of the spectacular new 203,000 square foot
Kansas Life Sciences Innovation Center on the University
of Kansas Medical Center Campus in Kansas City, Kansas began
in 2004 and was completed in 2007. The huge five-story building
now houses 80 state-of-the-art biosafety laboratories used
by physicians and scientists who conduct a wide range of
medical research. The adjoining laboratories are set up
along the north side of the building on all five floors
and in the center of the building (where specialized labs
are located). There are several common lab areas where researchers
can share equipment and collaborate. The tremendous volume
of lab work taking place during the day at this facility
required that a powerful and efficient laboratory exhaust
system be specified. Building designers also required that
all rooftop ventilation systems not detract from the building's
attractive appearance.
Greenheck's
Solution
- 12
Vektor-MD Laboratory Exhaust Systems
Greenheck's
Mixed Flow High Plume Dilution Blowers (Model Vektor-MD)
were selected and installed based on performance capabilities,
ease of installation, competitive pricing and their low-profile,
uniform appearance. Greenheck's Vektor-MDs are self-contained
exhaust systems specifically designed for hospital, pharmaceutical,
university, biotech and other laboratory applications. The
Vektor-MD employs a unique discharge nozzle design that
entrains additional ambient air to help dilute lab exhaust
fumes and then expels those fumes high above the lab building.
Two sizes of Vektor-MDs (Size 27 units are 14.25 feet high
and Size 36 units are 16 feet high) were selected for this
project to discharge air volumes of 41,000 cfms and 84,000
cfms and to achieve plume heights of 47 and 56 feet respectively.
As a result, diluted fumes discharged from the laboratories
will not contaminate the building's roof, re-enter make-up
air systems or drift down into surrounding neighborhoods.
The 12 Vektor-MD units installed on this project can easily
accommodate the 80 labs-even when all labs are in use at
one time. Because the sleek, low-profile appearance of the
Vector-MD units were installed on top of an attractive,
rooftop penthouse screen that houses other HVAC equipment.
Although somewhat difficult to reach at that location, maintenance
on the units will be minimal and will only require routine
motor replacement. Servicing motors will be safe and easy
because motor components are easily accessible outside the
contaminated exhaust air stream where the fan technology
is located.
The Results
-
Building managers and researchers are pleased with the
performance of the Greenheck Vektor-MD exhaust systems,
according to Don Rau, the director of facilities management
at the University of Kansas Medical Center. "The
Vektor fans atop the Kansas Life Sciences Innovation Center
certainly have performed well since the opening of the
facility," he said. ""There have been no
operational or performance issues. At this point we would
use the appropriate Vektor fans in any new research construction."
The mixed flow impeller technology provided by the Vektor-MD
units also has minimized energy consumption and overall
sound levels when compared to more traditional, custom-built
lab exhaust systems.
|
|